PDK API Guide for J721E
|
Histogram Module configuration Used to configure Histogram module Used to enable/disable histogram module.
Data Fields | |
uint32_t | enable |
uint32_t | input |
Fvid2_CropConfig | roi |
uint32_t Fcp_HistConfig::enable |
Flag to enable/disable histogram module TRUE: Enables histogram module, when enabled stores the output in two 256x2bit memory in ping-pong fashion FALSE: Disables histogram module
uint32_t Fcp_HistConfig::input |
Selects histogram input, Refer Fcp_HistInputSelect for valid values
Fvid2_CropConfig Fcp_HistConfig::roi |
Configures ROI for histogram