PDK API Guide for J721E
|
Input args for ENET_TIMESYNC_IOCTL_GET_ETH_RX_TIMESTAMP and ENET_TIMESYNC_IOCTL_GET_ETH_TX_TIMESTAMP commands.
Data Fields | |
EnetTimeSync_MsgType | msgType |
uint32_t | seqId |
uint32_t | portNum |
uint32_t | domain |
EnetTimeSync_MsgType EnetTimeSync_GetEthTimestampInArgs::msgType |
TimeSync event message type
uint32_t EnetTimeSync_GetEthTimestampInArgs::seqId |
Sequence id of the event
uint32_t EnetTimeSync_GetEthTimestampInArgs::portNum |
MAC port number corresponding to the event
uint32_t EnetTimeSync_GetEthTimestampInArgs::domain |
Domain number of the event