PDK API Guide for J721E
|
Config state machine variables. See IEEE Std 802.1Q-2018 8.6.8.4.
Data Fields | |
uint64_t | configChangeTime |
uint32_t | configChangeErrorCounter |
uint8_t | configPending |
uint8_t | configChange |
uint64_t EnetTas_ConfigStatus::configChangeTime |
New list is copied at this time.
uint32_t EnetTas_ConfigStatus::configChangeErrorCounter |
Config change error counter, incremented if admin->baseTime < current time and TAS_enabled is true.
uint8_t EnetTas_ConfigStatus::configPending |
True if list update is pending.
uint8_t EnetTas_ConfigStatus::configChange |
Set to true when application trigger updating of admin list to active list, cleared when configChangeTime is updated.