PDK API Guide for J721E
|
Enet RM IOCTL permission entry.
This structure has the information about IOCTL permissions for each IOCTL command.
Data Fields | |
uint32_t | cmd |
uint32_t | permittedCoreMask |
uint32_t EnetRm_IoctlPermissionEntry::cmd |
IOCTL command
uint32_t EnetRm_IoctlPermissionEntry::permittedCoreMask |
Cores from which this IOCTL call is allowed. This is a bitmask of allowed coreIds