PDK API Guide for J721E
|
Structure containing run time configuration of the display driver. This needs to be passed along with frame list to update any supported run time parameters.
Data Fields | |
Fvid2_PosConfig * | posCfg |
Dss_FrameRtParams * | inFrmParams |
Dss_FrameRtParams * | outFrmParams |
Dss_ScRtParams * | scParams |
Fvid2_PosConfig* Dss_DispRtParams::posCfg |
Position Configuration used to position the Frame in the Overlay. Refer to Fvid2_PosConfig for details. Note: Pass NULL if no change is required
Dss_FrameRtParams* Dss_DispRtParams::inFrmParams |
RT Params for input frame. This parameter is used to change the frame width and height at runtime. Note that this is used only when the buffer dimension is smaller than the LCD size. When changing the size, the application should ensure that the startX/startY + frame size doesn't exceed the display resolution. Refer to Dss_FrameRtParams for details. Note: Pass NULL if no change is required
Dss_FrameRtParams* Dss_DispRtParams::outFrmParams |
RT Params for output frame i.e. output of video pipeline. Only Width and height is valid in this structure. Refer to Dss_FrameRtParams for details. Note: Pass NULL if no change is required
Dss_ScRtParams* Dss_DispRtParams::scParams |
RT Params for scaler. Refer to Dss_ScRtParams for details. Note: Pass NULL if no change is required