PDK API Guide for J721E
|
Structure containing video pipe program callback parameters. This structure is used as an argument to IOCTL_DSS_DISP_REGISTER_PIPE_PRGM_CB.
Data Fields | |
Dss_DispPipePrgmCbFxn | pipePrgmCbFxn |
void * | appData |
Dss_DispPipePrgmCbFxn Dss_DispPipePrgmCbParams::pipePrgmCbFxn |
Application callback function to be called just after programming the hardware. A value of NULL will un-register the callback.
void* Dss_DispPipePrgmCbParams::appData |
Private data of application