PDK API Guide for J721E
|
Structure containing Safety Check configuration of Video Port. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_VP_SAFETY_CHK_PARAMS.
Data Fields | |
uint32_t | vpId |
uint32_t | safetySignSeedVal |
Dss_DctrlRegionSafetyChkCfg | regionSafetyChkCfg |
Dss_DctrlSafetyErrCbFxn | safetyErrCbFxn |
Dss_DctrlVpSafetyCbData | safetyCbData |
void * | appData |
uint32_t Dss_DctrlVpSafetyChkParams::vpId |
Video Port Id. See CSL_DssVpId for values
uint32_t Dss_DctrlVpSafetyChkParams::safetySignSeedVal |
Safety Signature Seed Value, only one non-zero value is possible in a particular context. In case user passes multiple non-zero values for different regions, previous value is overwritten.
Dss_DctrlRegionSafetyChkCfg Dss_DctrlVpSafetyChkParams::regionSafetyChkCfg |
Safety Check Configuration for a particular region. See Dss_DctrlRegionSafetyChkCfg for details
Dss_DctrlSafetyErrCbFxn Dss_DctrlVpSafetyChkParams::safetyErrCbFxn |
Safety Error callback function
Dss_DctrlVpSafetyCbData Dss_DctrlVpSafetyChkParams::safetyCbData |
Safety Error callback data to be returned to application
void* Dss_DctrlVpSafetyChkParams::appData |
Private data of application