PDK API Guide for J721E
|
Structure containing Error Stats of Video Port. This structure is used as an argument to IOCTL_DSS_DCTRL_GET_VP_ERROR_STATS.
Data Fields | |
uint32_t | vpId |
uint32_t | syncLost |
uint32_t | safetyViolation [CSL_DSS_VP_SAFETY_REGION_MAX] |
uint32_t | securityViolation |
uint32_t Dss_DctrlVpErrorStats::vpId |
Video Port Id. See CSL_DssVpId for values
uint32_t Dss_DctrlVpErrorStats::syncLost |
SyncLost Error Count of the LCD
uint32_t Dss_DctrlVpErrorStats::safetyViolation[CSL_DSS_VP_SAFETY_REGION_MAX] |
Safety Violation Count
uint32_t Dss_DctrlVpErrorStats::securityViolation |
Security Violation Count