PDK API Guide for J721E
|
This structure specifies the properties of the transfer for auto increment usecase.
Data Fields | |
uint16_t | sicnt0 |
uint16_t | sicnt1 |
uint16_t | sicnt2 |
uint16_t | sicnt3 |
int32_t | sdim1 |
int32_t | sdim2 |
int32_t | sdim3 |
uint16_t | dicnt0 |
uint16_t | dicnt1 |
uint16_t | dicnt2 |
uint16_t | dicnt3 |
int32_t | ddim1 |
int32_t | ddim2 |
int32_t | ddim3 |
uint16_t DmaUtilsAutoInc3d_TransferDim::sicnt0 |
Total loop iteration count for level 0 (innermost) for source
uint16_t DmaUtilsAutoInc3d_TransferDim::sicnt1 |
Total loop iteration count for level 1 for source
uint16_t DmaUtilsAutoInc3d_TransferDim::sicnt2 |
Total loop iteration count for level 2 for source
uint16_t DmaUtilsAutoInc3d_TransferDim::sicnt3 |
Total loop iteration count for level 3 for source
int32_t DmaUtilsAutoInc3d_TransferDim::sdim1 |
Jump in bytes when moving from from icnt0 to icnt1 for source
int32_t DmaUtilsAutoInc3d_TransferDim::sdim2 |
Jump in bytes when moving from from icnt1 to icnt2 for source
int32_t DmaUtilsAutoInc3d_TransferDim::sdim3 |
Jump in bytes when moving from from icnt2 to icnt3 for source
uint16_t DmaUtilsAutoInc3d_TransferDim::dicnt0 |
Total loop iteration count for level 0 (innermost) for destination
uint16_t DmaUtilsAutoInc3d_TransferDim::dicnt1 |
Total loop iteration count for level 1 for destination
uint16_t DmaUtilsAutoInc3d_TransferDim::dicnt2 |
Total loop iteration count for level 2 for destination
uint16_t DmaUtilsAutoInc3d_TransferDim::dicnt3 |
Total loop iteration count for level 3 for destination
int32_t DmaUtilsAutoInc3d_TransferDim::ddim1 |
Jump in bytes when moving from from icnt0 to icnt1 for destination
int32_t DmaUtilsAutoInc3d_TransferDim::ddim2 |
Jump in bytes when moving from from icnt1 to icnt2 for destination
int32_t DmaUtilsAutoInc3d_TransferDim::ddim3 |
Jump in bytes when moving from from icnt2 to icnt3 for destination