PDK API Guide for J721E
|
Data Fields | |
uint8_t * | trMem |
int32_t | trMemSize |
int32_t | numTRs |
int32_t | channelId |
uint8_t* DmaUtilsAutoInc3d_TrPrepareParam::trMem |
Allocated memory for TR descriptor, Use DmaUtilsAutoInc3d_getTrMemReq AP to know the actual size required for this memory
int32_t DmaUtilsAutoInc3d_TrPrepareParam::trMemSize |
Size of the memory allocated for trMem
int32_t DmaUtilsAutoInc3d_TrPrepareParam::numTRs |
Number of Transfer Records (TR's) that will be submitted to a particular channel
int32_t DmaUtilsAutoInc3d_TrPrepareParam::channelId |
channelId for which TR is prepared It is important to note that this id is a virtual id for channel and is not related to the actual channel used internally to do the transfer