PDK API Guide for J721E
|
CSIRX event status parameters. Instance of this structure will passed to the application call-back.
Data Fields | |
uint32_t | eventGroup |
uint32_t | eventMasks |
Fdrv_Handle | drvHandle |
uint32_t Csirx_EventStatus::eventGroup |
Event group from which event/s has happened. Refer CsirxDrv_EventGroup for event groups
uint32_t Csirx_EventStatus::eventMasks |
Events have occurred. Driver can set multiple flags depending on events happened Refer CsirxDrv_EventTypeError for Error events
Fdrv_Handle Csirx_EventStatus::drvHandle |
CSIRX driver handle pointer obtained during Fvid2_create()