PDK API Guide for J721E
|
Unicast entry type info apart from MAC address that can be set.
Data Fields | |
uint32_t | portNum |
bool | blocked |
bool | secure |
bool | super |
bool | ageable |
bool | trunk |
uint32_t CpswAle_UcastEntryInfo::portNum |
Port number that the packet with a unicast destination address is forwarded to
bool CpswAle_UcastEntryInfo::blocked |
Indicates that packet with a matching source or destination address should be dropped
bool CpswAle_UcastEntryInfo::secure |
Indicates that packet with a matching source address should be dropped, if the received port number is not equal to the port number in the table entry
bool CpswAle_UcastEntryInfo::super |
Indicates that this address can be received in port state other than Forwarding state
bool CpswAle_UcastEntryInfo::ageable |
Indicates if the unicast entry is subject to aging
bool CpswAle_UcastEntryInfo::trunk |
Indicates if the portNum refers to trunk number of port number