PDK API Guide for J721E
|
ALE classifier/policer match parameters.
Data Fields | |
uint32_t | policerMatchEnMask |
uint32_t | portNum |
bool | portIsTrunk |
uint32_t | priority |
CpswAle_OuiEntryInfo | ouiInfo |
CpswAle_MacAddrClassifierInfo | srcMacAddrInfo |
CpswAle_MacAddrClassifierInfo | dstMacAddrInfo |
uint32_t | ivlanId |
uint32_t | ovlanId |
uint16_t | etherType |
CpswAle_IpAddrClassifierInfo | srcIpInfo |
CpswAle_IpAddrClassifierInfo | dstIpInfo |
uint32_t CpswAle_PolicerMatchParams::policerMatchEnMask |
Bitmask selecting classifier types to enable.
uint32_t CpswAle_PolicerMatchParams::portNum |
Port number to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_PORT in policerMatchEnMask is set
bool CpswAle_PolicerMatchParams::portIsTrunk |
Flag indicating port number is a trunk group
uint32_t CpswAle_PolicerMatchParams::priority |
Received packet priority to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_PRIORITY in policerMatchEnMask is set
CpswAle_OuiEntryInfo CpswAle_PolicerMatchParams::ouiInfo |
OUI address to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_OUI in policerMatchEnMask is set
CpswAle_MacAddrClassifierInfo CpswAle_PolicerMatchParams::srcMacAddrInfo |
Source MAC address to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_MACSRC in policerMatchEnMask is set
CpswAle_MacAddrClassifierInfo CpswAle_PolicerMatchParams::dstMacAddrInfo |
Destination MAC address to match. Must valid if bit CPSW_ALE_POLICER_MATCH_MACDST in policerMatchEnMask is set
uint32_t CpswAle_PolicerMatchParams::ivlanId |
Inner VLAN ID to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_IVLAN in policerMatchEnMask is set
uint32_t CpswAle_PolicerMatchParams::ovlanId |
Outer VLAN ID to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_OVLAN in policerMatchEnMask is set
uint16_t CpswAle_PolicerMatchParams::etherType |
Frame EtherType to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_ETHERTYPE in policerMatchEnMask is set
CpswAle_IpAddrClassifierInfo CpswAle_PolicerMatchParams::srcIpInfo |
Source IP address to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_IPSRC in policerMatchEnMask is set
CpswAle_IpAddrClassifierInfo CpswAle_PolicerMatchParams::dstIpInfo |
Destination IP address to match. Must be valid if bit CPSW_ALE_POLICER_MATCH_IPDST in policerMatchEnMask is set