PDK API Guide for J721E
|
CSL_UdmapTR10 specifies a Type 10 Transfer Request.
Data Fields | |
uint32_t | flags |
uint16_t | icnt0 |
uint16_t | icnt1 |
uint64_t | addr |
int32_t | dim1 |
uint32_t | rsvd [3] |
uint32_t | fmtflags |
int32_t | ddim1 |
uint64_t | daddr |
uint32_t CSL_UdmapTR10::flags |
Specifies type of TR and how the TR should be handled. It also supports the TR triggering and output events.
uint16_t CSL_UdmapTR10::icnt0 |
Total loop iteration count for level 0 (innermost)
uint16_t CSL_UdmapTR10::icnt1 |
Total loop iteration count for level 1
uint64_t CSL_UdmapTR10::addr |
Starting address for the source data or destination data if it is a half duplex write
int32_t CSL_UdmapTR10::dim1 |
Signed dimension for loop level 1 for the source data
uint32_t CSL_UdmapTR10::rsvd[3] |
Reserved
uint32_t CSL_UdmapTR10::fmtflags |
Tells how the data is formatted either between the input and the output or if the data should use different addressing schemes or sizes
int32_t CSL_UdmapTR10::ddim1 |
Signed dimension for loop level 1 for the destination data
uint64_t CSL_UdmapTR10::daddr |
Starting address for the destination of the data