PDK API Guide for J721E
|
CSL_UdmapTR0 specifies a Type 0 (One dimensional data move) Transfer Request.
Data Fields | |
uint32_t | flags |
uint32_t | icnt0 |
uint64_t | addr |
uint32_t CSL_UdmapTR0::flags |
Specifies type of TR and how the TR should be handled. It also supports the TR triggering and output events.
uint32_t CSL_UdmapTR0::icnt0 |
Total loop iteration count for level 0 (innermost)
uint64_t CSL_UdmapTR0::addr |
Starting address for the source data or destination data if it is a half duplex write