PDK API Guide for J721E
|
Holds the EMAC statistics.
The statistics structure is the used to retrieve the current count of various packet events in the system. These values represent the delta values from the last time the statistics were read.
Uint32 CSL_CPSW_STATS::RxGoodFrames |
Good Frames Received
Uint32 CSL_CPSW_STATS::RxBCastFrames |
Good Broadcast Frames Received
Uint32 CSL_CPSW_STATS::RxMCastFrames |
Good Multicast Frames Received
Uint32 CSL_CPSW_STATS::RxPauseFrames |
PauseRx Frames Received
Uint32 CSL_CPSW_STATS::RxCRCErrors |
Frames Received with CRC Errors
Uint32 CSL_CPSW_STATS::RxAlignCodeErrors |
Frames Received with Alignment/Code Errors
Uint32 CSL_CPSW_STATS::RxOversized |
Oversized Frames Received
Uint32 CSL_CPSW_STATS::RxJabber |
Jabber Frames Received
Uint32 CSL_CPSW_STATS::RxUndersized |
Undersized Frames Received
Uint32 CSL_CPSW_STATS::RxFragments |
Rx Frame Fragments Received
Uint32 CSL_CPSW_STATS::RxAleDrop |
Rx frames dropped by the ALE
Uint32 CSL_CPSW_STATS::RxAleOverrunDrop |
Rx overrun frames dropped by the ALE
Uint32 CSL_CPSW_STATS::RxOctets |
Total Received Bytes in Good Frames
Uint32 CSL_CPSW_STATS::TxGoodFrames |
Good Frames Sent
Uint32 CSL_CPSW_STATS::TxBCastFrames |
Good Broadcast Frames Sent
Uint32 CSL_CPSW_STATS::TxMCastFrames |
Good Multicast Frames Sent
Uint32 CSL_CPSW_STATS::TxPauseFrames |
PauseTx Frames Sent
Uint32 CSL_CPSW_STATS::TxDeferred |
Frames Where Transmission was Deferred
Uint32 CSL_CPSW_STATS::TxCollision |
Total Frames Sent With Collision
Uint32 CSL_CPSW_STATS::TxSingleColl |
Frames Sent with Exactly One Collision
Uint32 CSL_CPSW_STATS::TxMultiColl |
Frames Sent with Multiple Colisions
Uint32 CSL_CPSW_STATS::TxExcessiveColl |
Tx Frames Lost Due to Excessive Collisions
Uint32 CSL_CPSW_STATS::TxLateColl |
Tx Frames Lost Due to a Late Collision
Uint32 CSL_CPSW_STATS::RxIpgError |
Rx inter-packet gap errors (10G only)
Uint32 CSL_CPSW_STATS::TxCarrierSLoss |
Tx Frames Lost Due to Carrier Sense Loss
Uint32 CSL_CPSW_STATS::TxOctets |
Total Transmitted Bytes in Good Frames
Uint32 CSL_CPSW_STATS::Frame64 |
Total Tx&Rx with Octet Size of 64
Uint32 CSL_CPSW_STATS::Frame65t127 |
Total Tx&Rx with Octet Size of 65 to 127
Uint32 CSL_CPSW_STATS::Frame128t255 |
Total Tx&Rx with Octet Size of 128 to 255
Uint32 CSL_CPSW_STATS::Frame256t511 |
Total Tx&Rx with Octet Size of 256 to 511
Uint32 CSL_CPSW_STATS::Frame512t1023 |
Total Tx&Rx with Octet Size of 512 to 1023
Uint32 CSL_CPSW_STATS::Frame1024tUp |
Total Tx&Rx with Octet Size of >=1024
Uint32 CSL_CPSW_STATS::NetOctets |
Sum of all Octets Tx or Rx on the Network
Uint32 CSL_CPSW_STATS::RxDropBottom |
Total Rx bottom of FIFO dropped frames
Uint32 CSL_CPSW_STATS::PortmaskFrop |
Total dropped frames due to portmask
Uint32 CSL_CPSW_STATS::RxDropTop |
Total Rx top of FIFO dropped frames
Uint32 CSL_CPSW_STATS::AleRateLimitDrop |
Total dropped frames due to ALE Rate Limiting
Uint32 CSL_CPSW_STATS::AleVidDrop |
Total dropped frames due to ALE VID Ingress
Uint32 CSL_CPSW_STATS::AleAddrEqDrop |
Total dropped frames due to DA=SA
Uint32 CSL_CPSW_STATS::Resv1[3] |
Unused Statistics registers
Uint32 CSL_CPSW_STATS::AleUnKnUni |
Total ALE Unknown Unicast frames
Uint32 CSL_CPSW_STATS::AleUnKnUniBytes |
Total ALE Unknown Unicast byte count
Uint32 CSL_CPSW_STATS::AleUnKnMulti |
Total ALE Unknown Multicast frames
Uint32 CSL_CPSW_STATS::AleUnKnMultiBytes |
Total ALE Unknown Multicast byte count
Uint32 CSL_CPSW_STATS::AleUnKnBCast |
Total ALE Unknown Broadcast frames
Uint32 CSL_CPSW_STATS::AleUnKnBCastBytes |
Total ALE Unknown Broadcast byte count
Uint32 CSL_CPSW_STATS::AlePolMatch |
Total ALE Policer Match frames
Uint32 CSL_CPSW_STATS::Resv2[46] |
Unused Statistics registers
Uint32 CSL_CPSW_STATS::TxMemProtectErr |
Total Tx Memory Protect CRC Error
Uint32 CSL_CPSW_STATS::TxPriPktCnt[8] |
Tx Priority [0-7] Packet Count
Uint32 CSL_CPSW_STATS::TxPriByteCnt[8] |
Tx Priority [0-7] Byte Count
Uint32 CSL_CPSW_STATS::TxPriDropPktCnt[8] |
Tx Priority [0-7] Drop packet Count
Uint32 CSL_CPSW_STATS::TxPriDropByteCnt[8] |
Tx Priority [0-7] Drop byte Count