PDK API Guide for J721E
|
Holds the CPSW_SS INTD version info.
Data Fields | |
Uint32 | scheme |
Uint32 | bu |
Uint32 | function |
Uint32 | rtlVer |
Uint32 | majorRevision |
Uint32 | custom |
Uint32 | minorRevision |
Uint32 CSL_CPSW_SS_INTD_VERSION::scheme |
Scheme value
Uint32 CSL_CPSW_SS_INTD_VERSION::bu |
BU value. Read as zero. Write have no effect
Uint32 CSL_CPSW_SS_INTD_VERSION::function |
Function value
Uint32 CSL_CPSW_SS_INTD_VERSION::rtlVer |
RTL version for instantiated IP
Uint32 CSL_CPSW_SS_INTD_VERSION::majorRevision |
Major revision
Uint32 CSL_CPSW_SS_INTD_VERSION::custom |
Custom value
Uint32 CSL_CPSW_SS_INTD_VERSION::minorRevision |
Minor revision