![]() |
PDK API Guide for J721E
|
Holds the ALE VLAN/Multicast Address Table entry configuration.
Data Fields | |
Uint8 | macAddress [6] |
Uint32 | vlanId |
Uint32 | mcastFwdState |
Uint32 | superEnable |
Uint32 | portMask |
Uint32 | ignMBits |
Uint8 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::macAddress[6] |
Multicast address
Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::vlanId |
VLAN Id
Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::mcastFwdState |
Multicast forward state
Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::superEnable |
Supervisory bit enable?
Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::portMask |
Port Mask.
Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::ignMBits |
Enable multicast address mask