PDK API Guide for J721E
|
Stream Monitor Line. Used to specify the byte and line numbers that will generate an interrupt. This register must only be modified when the corresponding line/byte enable is disabled.
Data Fields | |
uint16_t | lineCount |
uint16_t | byteCount |
uint16_t CSIRX_StreamMonitorLb::lineCount |
Indicates the line number to generate an interrupt. (First line of a Frame is line number 0)
uint16_t CSIRX_StreamMonitorLb::byteCount |
Indicates the byte number of the line to generate an interrupt. (First byte of a line is byte number 0)