PDK API Guide for J721E
|
Stream Frame Capture Counter control. Used to enable / disable the FCC and specify which virtual channel it should operate on.
Data Fields | |
uint16_t | frameCounter |
uint8_t | fccVc |
uint8_t | fccEn |
uint16_t CSIRX_StreamFccCtrl::frameCounter |
Current Frame number being processed
uint8_t CSIRX_StreamFccCtrl::fccVc |
Indicates which VC should be used to generate FCC interrupts. This value must not change while FccEn is enabled
uint8_t CSIRX_StreamFccCtrl::fccEn |
Frame Capture Counter enable.