PDK API Guide for J721E
|
This register provides information related to the current configuration. This should be read by FW to determine the number of streams available and other associated paramters that will influence how the device should be controlled.
Data Fields | |
uint8_t | monitorPresent [CSIRX_MAX_NUM_OF_STREAMS] |
uint8_t | numPixels [CSIRX_MAX_NUM_OF_STREAMS] |
uint8_t | fifoMode [CSIRX_MAX_NUM_OF_STREAMS] |
uint8_t | datapathSize |
uint8_t | numStreams |
uint8_t | cdnsPhyPresent |
uint8_t | maxLaneNb |
uint8_t | vcxConfig |
uint8_t | asfConfig |
uint8_t CSIRX_DeviceConfig::monitorPresent[CSIRX_MAX_NUM_OF_STREAMS] |
Pixel Monitor present
uint8_t CSIRX_DeviceConfig::numPixels[CSIRX_MAX_NUM_OF_STREAMS] |
The width of the pixel interface and the bits per pixel for the selected datatype will determine how many pixels can be output in a single cycle.
uint8_t CSIRX_DeviceConfig::fifoMode[CSIRX_MAX_NUM_OF_STREAMS] |
Stream FIFO Mode.
uint8_t CSIRX_DeviceConfig::datapathSize |
Internal Datapath width.
uint8_t CSIRX_DeviceConfig::numStreams |
Number of Stream interfaces.
uint8_t CSIRX_DeviceConfig::cdnsPhyPresent |
Cadence DPDHY present.
uint8_t CSIRX_DeviceConfig::maxLaneNb |
Max Number of Lanes.
uint8_t CSIRX_DeviceConfig::vcxConfig |
Extended Virtual Channel Configuration.
uint8_t CSIRX_DeviceConfig::asfConfig |
Additional Safety Features (ASF).