39 #ifndef SCICLIENT_SOC_TOP_H_ 40 #define SCICLIENT_SOC_TOP_H_ 46 #if defined (SOC_AM65XX) 47 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_resasg_types.h> 48 #include <ti/drv/sciclient/soc/V0/sciclient_fmwMsgParams.h> 49 #include <ti/drv/sciclient/soc/V0/sciclient_firmware_V0.h> 52 #if defined (SOC_J721E) 53 #include <ti/drv/sciclient/soc/sysfw/include/j721e/tisci_resasg_types.h> 58 #if defined (SOC_J7200) 59 #include <ti/drv/sciclient/soc/sysfw/include/j7200/tisci_resasg_types.h> 60 #include <ti/drv/sciclient/soc/V2/sciclient_fmwMsgParams.h> 61 #include <ti/drv/sciclient/soc/V2/sciclient_firmware_V2.h> 64 #if defined (SOC_AM64X) 65 #include <ti/drv/sciclient/soc/sysfw/include/am64x/tisci_resasg_types.h> 66 #include <ti/drv/sciclient/soc/V3/sciclient_fmwMsgParams.h> 67 #include <ti/drv/sciclient/soc/V3/sciclient_firmware_V3.h> 70 #if defined (SOC_J721S2) 71 #include <ti/drv/sciclient/soc/sysfw/include/j721s2/tisci_resasg_types.h> 72 #include <ti/drv/sciclient/soc/V4/sciclient_fmwMsgParams.h> 73 #include <ti/drv/sciclient/soc/V4/sciclient_firmware_V4-zebu.h> This file contains the definition of all the parameter IDs for PM, RM, Security.
File containing the Binary in a C array.