60 #ifndef SCICLIENT_DKEK_H_ 61 #define SCICLIENT_DKEK_H_ int32_t Sciclient_getDKEK(const struct tisci_msg_sa2ul_get_dkek_req *req, struct tisci_msg_sa2ul_get_dkek_resp *resp, uint32_t timeout)
Request for getting the firewall permissions.
TISCI Response for Releasing DKEK.
Definition: tisci_dkek.h:109
TISCI Response for setting DKEK in SA2UL registers.
Definition: tisci_dkek.h:90
TISCI Response for requesting DKEK.
Definition: tisci_dkek.h:137
int32_t Sciclient_setDKEK(const struct tisci_msg_sa2ul_set_dkek_req *req, struct tisci_msg_sa2ul_set_dkek_resp *resp, uint32_t timeout)
Request to derive a KEK and set SA2UL DKEK register.
TISCI Request for getting DKEK via TISCI.
Definition: tisci_dkek.h:124
int32_t Sciclient_releaseDKEK(const struct tisci_msg_sa2ul_release_dkek_req *req, struct tisci_msg_sa2ul_release_dkek_resp *resp, uint32_t timeout)
Request to erase the DKEK register.
TISCI Request for setting DKEK in SA2UL registers.
Definition: tisci_dkek.h:78
TISCI Request for releasing DKEK.
Definition: tisci_dkek.h:100