PDK API Guide for J721E
|
Functions | |
void | init_default_netif (void) |
Add Enet's netif and sets it as the default netif. More... | |
void | default_netif_poll (void) |
Run poll operation on default netif. More... | |
void | default_netif_shutdown (void) |
Remove Enet's netif. More... | |
void init_default_netif | ( | void | ) |
Add Enet's netif and sets it as the default netif.
void default_netif_poll | ( | void | ) |
Run poll operation on default netif.
This is an no-op for Enet's netif.
void default_netif_shutdown | ( | void | ) |
Remove Enet's netif.
Remote Enet's netif, which internally clears Enet's netif as lwIP's default netif.