This is Graph Configuration file
|
file | flexConnect_cfg.h |
| Defines the structures / control operations that could be used to configure / control Graph of VPAC.
|
|
|
struct | Fc_ErrEventParams |
| Structure for error event parameters Used to register callback for the given set of events. More...
|
|
|
typedef void(* | fc_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
| Prototype for the Error Event for Flex-connect. The callback for the Flex-connect error events can be registered using Fc_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs. More...
|
|
◆ fc_ErrEventCbFxn
typedef void(* fc_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
Prototype for the Error Event for Flex-connect. The callback for the Flex-connect error events can be registered using Fc_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs.
- Parameters
-
handle | FVID2 driver handle, for which error has occurred. |
errEvents | Error Events occured |
- Returns
- None.