PDK API Guide for J721E
|
The following definitions specify the driver operation environment that is defined by hardware configuration or client code. These defines are located in the header file of the core driver.
Macros | |
#define | CSITX_BPP_YUV_420_8_LEGACY (1.5) |
#define | CSITX_BPP_YUV_420_8 (1U) |
#define | CSITX_BPP_YUV_420_10 (1.25) |
#define | CSITX_BPP_YUV422_8 (2U) |
#define | CSITX_BPP_YUV422_10 (2.5) |
#define | CSITX_BPP_RGB888 (3U) |
#define | CSITX_BPP_RGB666 (2.25) |
#define | CSITX_BPP_RGB565 (2U) |
#define | CSITX_BPP_RGB555 (2U) |
#define | CSITX_BPP_RGB444 (2U) |
#define | CSITX_MAGIC_NUMBER 0x50250300U |
#define CSITX_BPP_YUV_420_8_LEGACY (1.5) |
Bytes per pixel values for the supported pixel formats
YUV420 8-bit (legacy)
#define CSITX_BPP_YUV_420_8 (1U) |
YUV420 8-bit
#define CSITX_BPP_YUV_420_10 (1.25) |
YUV420 10-bit
#define CSITX_BPP_YUV422_8 (2U) |
YUV422 8-bit
#define CSITX_BPP_YUV422_10 (2.5) |
YUV422 10-bit
#define CSITX_BPP_RGB888 (3U) |
RGB888
#define CSITX_BPP_RGB666 (2.25) |
RGB666
#define CSITX_BPP_RGB565 (2U) |
RGB565
#define CSITX_BPP_RGB555 (2U) |
RGB555
#define CSITX_BPP_RGB444 (2U) |
RGB444
#define CSITX_MAGIC_NUMBER 0x50250300U |
Magic number value