PDK API Guide for J721E

Introduction

Functions

static uint32_t CSL_udmapCppi5GetDescType (const void *pDesc)
 Get the descriptor type. More...
 
static void CSL_udmapCppi5SetDescType (void *pDesc, uint32_t descType)
 Set the descriptor type. More...
 
static uint32_t CSL_udmapCppi5GetPktLen (const void *pDesc)
 Get the packet length. More...
 
static void CSL_udmapCppi5SetPktLen (void *pDesc, uint32_t descType, uint32_t pktLen)
 Set the packet length. More...
 
static void CSL_udmapCppi5HostSetPktLen (void *pDesc, uint32_t pktLen)
 Set the packet length of host mode packet descriptors. More...
 
static void CSL_udmapCppi5MonoSetPktLen (void *pDesc, uint32_t pktLen)
 Set the packet length of mono mode packet descriptors. More...
 
static void CSL_udmapCppi5TrSetPktLen (void *pDesc, uint32_t pktLen)
 Set the packet length of TR mode packet descriptors. More...
 
static uint64_t CSL_udmapCppi5GetBufferAddr (const CSL_UdmapCppi5HMPD *pDesc)
 Get the buffer address. More...
 
static uint32_t CSL_udmapCppi5GetBufferLen (const CSL_UdmapCppi5HMPD *pDesc)
 Get the buffer length. More...
 
static void CSL_udmapCppi5SetBufferAddr (CSL_UdmapCppi5HMPD *pDesc, uint64_t physBufferAddr)
 Set the buffer address. More...
 
static void CSL_udmapCppi5SetOrgBufferAddr (CSL_UdmapCppi5HMPD *pDesc, uint64_t physBufferAddr)
 Set the original buffer address. More...
 
static void CSL_udmapCppi5SetBufferLen (CSL_UdmapCppi5HMPD *pDesc, uint32_t bufferLenBytes)
 Set the buffer length. More...
 
static void CSL_udmapCppi5SetOrgBufferLen (CSL_UdmapCppi5HMPD *pDesc, uint32_t bufferLenBytes)
 Set the original buffer length. More...
 
static void CSL_udmapCppi5LinkDesc (CSL_UdmapCppi5HMPD *pDesc, uint64_t physBufferDescAddr)
 Link a buffer descriptor to a descriptor. More...
 
static bool CSL_udmapCppi5IsEpiDataPresent (const void *pDesc)
 Is the EPI block present in the descriptor? More...
 
static void CSL_udmapCppi5SetEpiDataPresent (void *pDesc, bool bEpiDataPresent)
 Set indicator if the EPI block is present in the descriptor. More...
 
static uint32_t * CSL_udmapCppi5GetEpiDataPtr (const void *pDesc)
 Return pointer to EPI block data. More...
 
static int32_t CSL_udmapCppi5RdEpiData (const void *pDesc, uint32_t *pTsInfo, uint32_t *pSwInfo0, uint32_t *pSwInfo1, uint32_t *pSwInfo2)
 Read the EPI block data. More...
 
static void CSL_udmapCppi5WrEpiData (const void *pDesc, uint32_t tsInfo, uint32_t swInfo0, uint32_t swInfo1, uint32_t swInfo2)
 Write the EPI block data. More...
 
static uint32_t CSL_udmapCppi5GetPsDataLoc (const void *pDesc)
 Get the location of the protocol-specific data. More...
 
static void CSL_udmapCppi5SetPsDataLoc (void *pDesc, uint32_t psLoc)
 Set the location of the protocol-specific data. More...
 
static uint32_t CSL_udmapCppi5GetPsDataLen (const void *pDesc)
 Get the number of bytes of protocol-specific data. More...
 
static void CSL_udmapCppi5SetPsDataLen (void *pDesc, uint32_t psDataLen)
 Set the number of bytes of protocol-specific data. More...
 
static uint64_t CSL_udmapCppi5GetPsDataAddr (const void *pDesc, bool bInSopBuf, bool bEpiPresent)
 Return address of the protocol-specific data. More...
 
static uint8_t * CSL_udmapCppi5GetPsDataPtr (const void *pDesc)
 
static uint32_t CSL_udmapCppi5GetSrcTag (const void *pDesc)
 Get source tag. More...
 
static uint32_t CSL_udmapCppi5GetDstTag (const void *pDesc)
 Get destination tag. More...
 
static void CSL_udmapCppi5SetSrcTag (void *pDesc, uint32_t srcTag)
 Set source tag. More...
 
static void CSL_udmapCppi5SetDstTag (void *pDesc, uint32_t dstTag)
 Set destination tag. More...
 
static uint32_t CSL_udmapCppi5GetErrorFlags (const void *pDesc)
 Get error flags. More...
 
static uint32_t CSL_udmapCppi5GetPsFlags (const void *pDesc)
 Get ps flags. More...
 
static void CSL_udmapCppi5SetPsFlags (void *pDesc, uint32_t psFlags)
 Set ps flags. More...
 
static uint32_t CSL_udmapCppi5GetPktType (const void *pDesc)
 Get packet type. More...
 
static void CSL_udmapCppi5SetPktType (void *pDesc, uint32_t pktType)
 Set packet type. More...
 
static void CSL_udmapCppi5GetIds (const void *pDesc, uint32_t *pPktId, uint32_t *pFlowId)
 Get IDs. More...
 
static void CSL_udmapCppi5SetIds (void *pDesc, uint32_t descType, uint32_t pktId, uint32_t flowId)
 Set IDs. More...
 
static void CSL_udmapCppi5GetReturnPolicy (const void *pDesc, uint32_t *pRetPolicy, uint32_t *pEarlyReturn, uint32_t *pRetPushPolicy, uint32_t *pRetQnum)
 Get descriptor return policy information. More...
 
static void CSL_udmapCppi5SetReturnPolicy (void *pDesc, uint32_t descType, uint32_t retPolicy, uint32_t earlyReturn, uint32_t retPushPolicy, uint32_t retQnum)
 Set descriptor return policy information. More...
 
static uint32_t CSL_udmapCppi5MonoGetDataOffset (const CSL_UdmapCppi5MMPD *pDesc)
 Get MONO descriptor data offset. More...
 
static void CSL_udmapCppi5MonoSetDataOffset (CSL_UdmapCppi5MMPD *pDesc, uint32_t dataOffset)
 Set MONO descriptor data offset. More...
 
static void CSL_udmapCppi5TrGetReload (const CSL_UdmapCppi5TRPD *pDesc, uint32_t *pReloadEnable, uint32_t *pReloadIdx)
 Get TR descriptor reload information. More...
 
static void CSL_udmapCppi5TrSetReload (CSL_UdmapCppi5TRPD *pDesc, uint32_t reloadEnable, uint32_t reloadIdx)
 Set TR descriptor reload information. More...
 
static uint32_t CSL_udmapCppi5TrGetEntryStride (const CSL_UdmapCppi5TRPD *pDesc)
 Get TR descriptor entry stride. More...
 
static void CSL_udmapCppi5TrSetEntryStride (CSL_UdmapCppi5TRPD *pDesc, uint32_t entryStride)
 Set TR descriptor entry stride. More...
 

Function Documentation

◆ CSL_udmapCppi5GetDescType()

static uint32_t CSL_udmapCppi5GetDescType ( const void *  pDesc)
inlinestatic

Get the descriptor type.

This function returns the type of descriptor. Valid descriptor types are: 1 = Host-mode (HOST) packet descriptor 2 = Monolithic-mode (MONO) packet descriptor 3 = Transfer Request mode (TR) packet descriptor

Parameters
pDesc[IN] Pointer to the descriptor
Returns
Descriptor type

◆ CSL_udmapCppi5SetDescType()

static void CSL_udmapCppi5SetDescType ( void *  pDesc,
uint32_t  descType 
)
inlinestatic

Set the descriptor type.

This function sets the type of descriptor. Valid descriptor types are: 1 = Host-mode (HOST) packet descriptor 2 = Monolithic-mode (MONO) packet descriptor 3 = Transfer Request mode (TR) packet descriptor

Note that no error checking is performed on the passed descriptor type argument.

Parameters
pDesc[IN] Pointer to the descriptor
descType[IN] Descriptor type
Returns
None

◆ CSL_udmapCppi5GetPktLen()

static uint32_t CSL_udmapCppi5GetPktLen ( const void *  pDesc)
inlinestatic

Get the packet length.

This function returns the packet length. The value returned depends on the type of descriptor as follows:

Host and mono mode packet descriptors: The length of the packet in bytes is returned

TR mode packet descriptors: The number of TRs in the packet is returned

Parameters
pDesc[IN] Pointer to the descriptor
Returns
Packet length

◆ CSL_udmapCppi5SetPktLen()

static void CSL_udmapCppi5SetPktLen ( void *  pDesc,
uint32_t  descType,
uint32_t  pktLen 
)
inlinestatic

Set the packet length.

This function sets the packet length. The meaning of the pktLen argument depends on the type of descriptor as follows:

Host and mono mode packet descriptors: pktLen = the length of the packet in bytes

TR mode packet descriptors: pktlen = the number of TRs in the packet

Parameters
pDesc[IN] Pointer to the descriptor
descType[IN] Descriptor type
pktLen[IN] Packet length
Returns
None

◆ CSL_udmapCppi5HostSetPktLen()

static void CSL_udmapCppi5HostSetPktLen ( void *  pDesc,
uint32_t  pktLen 
)
inlinestatic

Set the packet length of host mode packet descriptors.

This function sets the packet length of host packet descriptors.

Parameters
pDesc[IN] Pointer to the descriptor
pktLen[IN] Packet length in bytes
Returns
None

◆ CSL_udmapCppi5MonoSetPktLen()

static void CSL_udmapCppi5MonoSetPktLen ( void *  pDesc,
uint32_t  pktLen 
)
inlinestatic

Set the packet length of mono mode packet descriptors.

This function sets the packet length of mono mode packet descriptors.

Parameters
pDesc[IN] Pointer to the descriptor
pktLen[IN] Packet length in bytes
Returns
None

◆ CSL_udmapCppi5TrSetPktLen()

static void CSL_udmapCppi5TrSetPktLen ( void *  pDesc,
uint32_t  pktLen 
)
inlinestatic

Set the packet length of TR mode packet descriptors.

This function sets the packet length of TR mode packet descriptors.

Parameters
pDesc[IN] Pointer to the descriptor
pktLen[IN] Number of TRs in the packet
Returns
None

◆ CSL_udmapCppi5GetBufferAddr()

static uint64_t CSL_udmapCppi5GetBufferAddr ( const CSL_UdmapCppi5HMPD pDesc)
inlinestatic

Get the buffer address.

This function returns the physical address of the buffer attached to the specified descriptor.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
Returns
Physical address of the buffer

◆ CSL_udmapCppi5GetBufferLen()

static uint32_t CSL_udmapCppi5GetBufferLen ( const CSL_UdmapCppi5HMPD pDesc)
inlinestatic

Get the buffer length.

This function returns the length of the buffer (in bytes) attached to the specified descriptor.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
Returns
Length of the buffer in bytes

◆ CSL_udmapCppi5SetBufferAddr()

static void CSL_udmapCppi5SetBufferAddr ( CSL_UdmapCppi5HMPD pDesc,
uint64_t  physBufferAddr 
)
inlinestatic

Set the buffer address.

This function writes the physical address of the buffer to the specified descriptor. This function is useful when configuring host-mode descriptors/buffers to be placed on a transmit queue.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
physBufferAddr[IN] Physical address of the buffer
Returns
None

◆ CSL_udmapCppi5SetOrgBufferAddr()

static void CSL_udmapCppi5SetOrgBufferAddr ( CSL_UdmapCppi5HMPD pDesc,
uint64_t  physBufferAddr 
)
inlinestatic

Set the original buffer address.

This function writes the original physical address of the buffer to the specified descriptor. This function is useful when initializing host-mode descriptors/buffers to be placed on transmit or receive free queues.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
physBufferAddr[IN] Physical address of the buffer
Returns
None

◆ CSL_udmapCppi5SetBufferLen()

static void CSL_udmapCppi5SetBufferLen ( CSL_UdmapCppi5HMPD pDesc,
uint32_t  bufferLenBytes 
)
inlinestatic

Set the buffer length.

This function writes the buffer length (in bytes) to the specified descriptor. This function is useful when configuring host-mode descriptors/buffers to be placed on a transmit queue.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
bufferLenBytes[IN] Length of the buffer in bytes
Returns
None

◆ CSL_udmapCppi5SetOrgBufferLen()

static void CSL_udmapCppi5SetOrgBufferLen ( CSL_UdmapCppi5HMPD pDesc,
uint32_t  bufferLenBytes 
)
inlinestatic

Set the original buffer length.

This function writes the original buffer length (in bytes) to the specified descriptor. This function is useful when initializing host-mode descriptors/buffers to be placed on transmit or receive free queues.

This function is intended for use with host-mode descriptors only.

Parameters
pDesc[IN] Pointer to the host-mode descriptor
bufferLenBytes[IN] Length of the buffer in bytes
Returns
None

◆ CSL_udmapCppi5LinkDesc()

static void CSL_udmapCppi5LinkDesc ( CSL_UdmapCppi5HMPD pDesc,
uint64_t  physBufferDescAddr 
)
inlinestatic

Link a buffer descriptor to a descriptor.

This function links a buffer descriptor to the specified descriptor (which can be either a packet descriptor or a buffer descriptor).

This function is intended for use with host-mode descriptors only.

Note that the physical address of the buffer descriptor being linked must be provided. It is also assumed that the caller has initialized all required fields of the buffer descriptor prior to linking it.

Parameters
pDesc[IN] Pointer to the descriptor being linked to
physBufferDescAddr[IN] Physical address of the buffer descriptor being linked
Returns
None

◆ CSL_udmapCppi5IsEpiDataPresent()

static bool CSL_udmapCppi5IsEpiDataPresent ( const void *  pDesc)
inlinestatic

Is the EPI block present in the descriptor?

This function returns true if the Extended Packet Info (EPI) block is present in the descriptor and false if it is not present.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
true = EPI block is present in the descriptor false = EPI block is not present in the descriptor

◆ CSL_udmapCppi5SetEpiDataPresent()

static void CSL_udmapCppi5SetEpiDataPresent ( void *  pDesc,
bool  bEpiDataPresent 
)
inlinestatic

Set indicator if the EPI block is present in the descriptor.

This function is used to set if the Extended Packet Info (EPI) block is present in the descriptor (true) or if it is not present (false).

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
bEpiDataPresent[IN] true if EPI block is present, false if not
Returns
None

◆ CSL_udmapCppi5GetEpiDataPtr()

static uint32_t * CSL_udmapCppi5GetEpiDataPtr ( const void *  pDesc)
inlinestatic

Return pointer to EPI block data.

This function returns a pointer to the Extended Packet Info (EPI) block data within the descriptor. If the EPI block is not present, NULL is returned.

This function only operates on host-mode and mono-mode descriptors.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
A pointer to the EPI block data within the descriptor is returned, or NULL is the EPI block is not present in the descriptor

◆ CSL_udmapCppi5RdEpiData()

static int32_t CSL_udmapCppi5RdEpiData ( const void *  pDesc,
uint32_t *  pTsInfo,
uint32_t *  pSwInfo0,
uint32_t *  pSwInfo1,
uint32_t *  pSwInfo2 
)
inlinestatic

Read the EPI block data.

This function reads and returns the Extended Packet Info (EPI) block data within the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
pTsInfo[OUT] Pointer where to store Timestamp information
*pSwInfo0[OUT] Pointer where to store Software information word 0
*pSwInfo1[OUT] Pointer where to store Software information word 1
*pSwInfo2[OUT] Pointer where to store Software information word 2
Returns
0 = success -1 = No EPI block data is present in the descriptor

◆ CSL_udmapCppi5WrEpiData()

static void CSL_udmapCppi5WrEpiData ( const void *  pDesc,
uint32_t  tsInfo,
uint32_t  swInfo0,
uint32_t  swInfo1,
uint32_t  swInfo2 
)
inlinestatic

Write the EPI block data.

This function writes the Extended Packet Info (EPI) block data into the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
tsInfo[IN] Timestamp information
swInfo0[IN] Software information word 0
swInfo1[IN] Software information word 1
swInfo2[IN] Software information word 2
Returns
None

◆ CSL_udmapCppi5GetPsDataLoc()

static uint32_t CSL_udmapCppi5GetPsDataLoc ( const void *  pDesc)
inlinestatic

Get the location of the protocol-specific data.

This function returns the location of the protocol-specific data.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
0 = Protocol-specific data is in the descriptor 1 = Protocol-specific data is in the SOP buffer

◆ CSL_udmapCppi5SetPsDataLoc()

static void CSL_udmapCppi5SetPsDataLoc ( void *  pDesc,
uint32_t  psLoc 
)
inlinestatic

Set the location of the protocol-specific data.

This function sets the location of the protocol-specific data.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
psLoc[IN] 0 = Protocol-specific data is in the descriptor 1 = Protocol-specific data is in the SOP buffer
Returns
None

◆ CSL_udmapCppi5GetPsDataLen()

static uint32_t CSL_udmapCppi5GetPsDataLen ( const void *  pDesc)
inlinestatic

Get the number of bytes of protocol-specific data.

This function returns the number of bytes of protocol-specific (ps) data present in the descriptor. This value will be a multiple of 4.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
The number of bytes of ps data is returned

◆ CSL_udmapCppi5SetPsDataLen()

static void CSL_udmapCppi5SetPsDataLen ( void *  pDesc,
uint32_t  psDataLen 
)
inlinestatic

Set the number of bytes of protocol-specific data.

This function sets the number of bytes of protocol-specific (ps) data present in the descriptor or SOP buffer. This value must be a multiple of 4.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
psDataLen[IN] Number of bytes of protocol-specific (ps) data present in the descriptor or SOP buffer
Returns
None

◆ CSL_udmapCppi5GetPsDataAddr()

static uint64_t CSL_udmapCppi5GetPsDataAddr ( const void *  pDesc,
bool  bInSopBuf,
bool  bEpiPresent 
)
inlinestatic

Return address of the protocol-specific data.

This function returns the address of the protocol-specific data within the descriptor or SOP buffer.

If the protocol-specific data is in the descriptor (bInDesc is true), the address returned is a virtual address. If the protocol-specific data is in the SOP buffer (bInDesc is false), the address returned is a physical address.

This function only operates on host-mode and mono-mode descriptors.

Parameters
pDesc[IN] Pointer to the descriptor
bInSopBuf[IN] true if ps data is in SOP buffer, false otherwise
bEpiPresent[IN] true if EPI data is present, false otherwise
Returns
Address of the protocol-specific data

◆ CSL_udmapCppi5GetPsDataPtr()

static uint8_t * CSL_udmapCppi5GetPsDataPtr ( const void *  pDesc)
inlinestatic

◆ CSL_udmapCppi5GetSrcTag()

static uint32_t CSL_udmapCppi5GetSrcTag ( const void *  pDesc)
inlinestatic

Get source tag.

This function gets the source tag from the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
Source tag

◆ CSL_udmapCppi5GetDstTag()

static uint32_t CSL_udmapCppi5GetDstTag ( const void *  pDesc)
inlinestatic

Get destination tag.

This function gets the destination tag from the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
Destination tag

◆ CSL_udmapCppi5SetSrcTag()

static void CSL_udmapCppi5SetSrcTag ( void *  pDesc,
uint32_t  srcTag 
)
inlinestatic

Set source tag.

This function sets the source tag in the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
srcTag[IN] source tag
Returns
None

◆ CSL_udmapCppi5SetDstTag()

static void CSL_udmapCppi5SetDstTag ( void *  pDesc,
uint32_t  dstTag 
)
inlinestatic

Set destination tag.

This function sets the destination tag in the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
dstTag[IN] destination tag
Returns
None

◆ CSL_udmapCppi5GetErrorFlags()

static uint32_t CSL_udmapCppi5GetErrorFlags ( const void *  pDesc)
inlinestatic

Get error flags.

This function gets the error flags from the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
The error flags are returned

◆ CSL_udmapCppi5GetPsFlags()

static uint32_t CSL_udmapCppi5GetPsFlags ( const void *  pDesc)
inlinestatic

Get ps flags.

This function gets the protocol-specific (ps) flags from the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
The protocol-specific (ps) flags are returned

◆ CSL_udmapCppi5SetPsFlags()

static void CSL_udmapCppi5SetPsFlags ( void *  pDesc,
uint32_t  psFlags 
)
inlinestatic

Set ps flags.

This function sets the protocol-specific (ps) flags in the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
psFlags[IN] ps flags
Returns
None

◆ CSL_udmapCppi5GetPktType()

static uint32_t CSL_udmapCppi5GetPktType ( const void *  pDesc)
inlinestatic

Get packet type.

This function gets the packet type from the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
Returns
Packet type

◆ CSL_udmapCppi5SetPktType()

static void CSL_udmapCppi5SetPktType ( void *  pDesc,
uint32_t  pktType 
)
inlinestatic

Set packet type.

This function sets the packet type in the descriptor.

This function is intended for use with host-mode and mono-mode descriptors only.

Parameters
pDesc[IN] Pointer to the descriptor
pktType[IN] Packet type
Returns
None

◆ CSL_udmapCppi5GetIds()

static void CSL_udmapCppi5GetIds ( const void *  pDesc,
uint32_t *  pPktId,
uint32_t *  pFlowId 
)
inlinestatic

Get IDs.

This function gets the packet ID and flow ID from the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
pPktId[OUT] Pointer where to store packet ID
pFlowId[OUT] Pointer where to store flow ID
Returns
None

◆ CSL_udmapCppi5SetIds()

static void CSL_udmapCppi5SetIds ( void *  pDesc,
uint32_t  descType,
uint32_t  pktId,
uint32_t  flowId 
)
inlinestatic

Set IDs.

This function sets the packet ID and flow ID in the descriptor.

Parameters
pDesc[IN] Pointer to the descriptor
descType[IN] Descriptor type
pktId[IN] packet ID
flowId[IN] flow ID
Returns
None

◆ CSL_udmapCppi5GetReturnPolicy()

static void CSL_udmapCppi5GetReturnPolicy ( const void *  pDesc,
uint32_t *  pRetPolicy,
uint32_t *  pEarlyReturn,
uint32_t *  pRetPushPolicy,
uint32_t *  pRetQnum 
)
inlinestatic

Get descriptor return policy information.

This function gets descriptor return policy information from the descriptor. See CSL_udmapCppi5SetReturnPolicy for a description of the return policy information.

Parameters
pDesc[IN] Pointer to the descriptor
pRetPolicy[OUT] Pointer where to store return policy (0 is returned for MONO and TR descriptor types)
pEarlyReturn[OUT] Pointer where to store early return (0 is returned for TR descriptor type)
pRetPushPolicy[OUT] Pointer where to store return push policy
pRetQnum[OUT] Pointer where to store return queue #
Returns
None

◆ CSL_udmapCppi5SetReturnPolicy()

static void CSL_udmapCppi5SetReturnPolicy ( void *  pDesc,
uint32_t  descType,
uint32_t  retPolicy,
uint32_t  earlyReturn,
uint32_t  retPushPolicy,
uint32_t  retQnum 
)
inlinestatic

Set descriptor return policy information.

This function sets descriptor return policy information in the descriptor. This includes the following:

return policy (HOST descriptor type only) 0 = Entire packet (still linked together) should be returned to queue specified by pRetQnum 1 = Each descriptor should be returned to queue specified by pRetQnum in their respective descriptors.

early return (HOST and MONO descriptor types only) 0 = Buffer/packet descriptor pointers should only be returned after all reads have been completed 1 = Buffer/packet descriptor pointers should be returned immediately upon fetching the descriptor and beginning to transfer data

return push policy (only used when return policy is 1) 0 = Descriptor is returned to tail of queue 1 = Descriptor is returned to head of queue

return queue # Specifies the queue / ring number that the descriptor is returned to after transmission is complete.

Parameters
pDesc[IN] Pointer to the descriptor
descType[IN] Descriptor type
retPolicy[IN] return policy (only used for HOST descriptor type)
earlyReturn[IN] early return (only used for HOST and MONO descriptor types)
retPushPolicy[IN] return push policy
retQnum[IN] return queue #
Returns
None

◆ CSL_udmapCppi5MonoGetDataOffset()

static uint32_t CSL_udmapCppi5MonoGetDataOffset ( const CSL_UdmapCppi5MMPD pDesc)
inlinestatic

Get MONO descriptor data offset.

This function returns the data offset for a monolithic-mode (MONO) type of descriptor. This value indicates the byte offset from byte 0 of the descriptor to the location where the valid data begins.

Parameters
pDesc[IN] Pointer to the MONO descriptor
Returns
Byte offset from start of descriptor to valid data

◆ CSL_udmapCppi5MonoSetDataOffset()

static void CSL_udmapCppi5MonoSetDataOffset ( CSL_UdmapCppi5MMPD pDesc,
uint32_t  dataOffset 
)
inlinestatic

Set MONO descriptor data offset.

This function sets the data offset for a monolithic-mode (MONO) type of descriptor. This value indicates the byte offset from byte 0 of the descriptor to the location where the valid data begins.

Parameters
pDesc[IN] Pointer to the MONO descriptor
dataOffset[IN] Byte offset
Returns
None

◆ CSL_udmapCppi5TrGetReload()

static void CSL_udmapCppi5TrGetReload ( const CSL_UdmapCppi5TRPD pDesc,
uint32_t *  pReloadEnable,
uint32_t *  pReloadIdx 
)
inlinestatic

Get TR descriptor reload information.

This function returns reload information for a transfer-request (TR) type of descriptor. See CSL_udmapCppi5TrSetReload for a description of this reload information.

Parameters
pDesc[IN] Pointer to the TR descriptor
pReloadEnable[OUT] Pointer where to store reload enable
pReloadIdx[OUT] Pointer where to store reload index
Returns
None

◆ CSL_udmapCppi5TrSetReload()

static void CSL_udmapCppi5TrSetReload ( CSL_UdmapCppi5TRPD pDesc,
uint32_t  reloadEnable,
uint32_t  reloadIdx 
)
inlinestatic

Set TR descriptor reload information.

This function sets reload information for a transfer-request (TR) type of descriptor. Reload information includes:

reload enable (specifies what to do when the last entry is processed in this packet) 0 = Finish the packet and place the descriptor back on the return queue 1 = Vector to the Reload Index and resume processing

reload index Specifies the value to set the current processing index to when the last entry is processed and reload enable is set to 1. This is basically an absolute index to jump to on the 2nd and following passes through the TR packet.

Parameters
pDesc[IN] Pointer to the TR descriptor
reloadEnable[IN] reload enable
reloadIdx[IN] reload index
Returns
None

◆ CSL_udmapCppi5TrGetEntryStride()

static uint32_t CSL_udmapCppi5TrGetEntryStride ( const CSL_UdmapCppi5TRPD pDesc)
inlinestatic

Get TR descriptor entry stride.

This function returns the stride between TR entries. See CSL_udmapCppi5TrSetEntryStride for valid stride values.

Parameters
pDesc[IN] Pointer to the TR descriptor
Returns
Encoded TR entry stride

◆ CSL_udmapCppi5TrSetEntryStride()

static void CSL_udmapCppi5TrSetEntryStride ( CSL_UdmapCppi5TRPD pDesc,
uint32_t  entryStride 
)
inlinestatic

Set TR descriptor entry stride.

This function sets the stride between TR entries. This value must be set large enough that any TR in the buffer will fit within the given dimension. TRs are expected to be placed on boundaries as given in this dimension.

The stride value is encoded as follows: 0 = 16 byte TR entry 1 = 32-byte TR entry 2 = 64-byte TR entry 3 = 128-byte TR entry

Parameters
pDesc[IN] Pointer to the TR descriptor
entryStride[IN] Encoded TR entry stride
Returns
None