PDK API Guide for J721E
|
The CPSW statistics module implements only the IOCTLs defined in the generic Enet Statistics API. There are no additional CPSW-specific IOCTLs.
The statistics structures are CPSW specific and may vary depending on the CPSW instance:
Interrupts:
Data Structures | |
struct | CpswStats_HostPort_2g |
CPSW 2G host port statistics. More... | |
struct | CpswStats_MacPort_2g |
CPSW 2G MAC port statistics. More... | |
struct | CpswStats_HostPort_Ng |
CPSW 5G or 9G host port statistics. More... | |
struct | CpswStats_MacPort_Ng |
CPSW 5G or 9G MAC port statistics. More... | |
struct | CpswStats_PortStats |
CPSW nG port statistics. More... | |
Macros | |
#define | CPSW_STATS_BLOCK_ELEM_NUM (128U) |
Number of elements in a statistics block. More... | |
#define CPSW_STATS_BLOCK_ELEM_NUM (128U) |
Number of elements in a statistics block.