PDK API Guide for J721E
|
Data Structures | |
struct | Board_IDInfo |
This structure contains board specific information. More... | |
struct | __attribute__ |
This structure contains board specific information. More... | |
struct | Board_SoCInfo |
This structure contains SoC specific information. More... | |
Typedefs | |
typedef uint32_t | Board_initCfg |
typedef void(* | Board_thermalMgmtCallbackFunction_t) (Board_DDRTempEventType DDRTempEventType) |
Enumerations | |
enum | Board_DDRTempEventType { BOARD_DDR_TEMP_EVENT_TEMP_ALERT = 1, BOARD_DDR_TEMP_EVENT_LOW_TEMP_ALARM = 2, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_4X_REFRESH = 3, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_2X_REFRESH = 4, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_1X_REFRESH = 5, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_1_BY_2_REFRESH = 6, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_1_BY_4_REFRESH = 7, BOARD_DDR_TEMP_EVENT_TEMP_CHANGE_1_BY_4_REFRESH_WITH_DERATING = 8, BOARD_DDR_TEMP_EVENT_HIGH_TEMP_ALARM = 9 } |
Enumeration of reported temperature event types. More... | |
#define BOARD_CACHE_LINE_SIZE (128) |
Board Library uses basic C99 data types. The basic types used are uint32_t, int32_t, uint8_t, int8_t, uint16_t and int16_t. The standard C char is used for strings. Complex types (or typdefs) if used are defined within this header file.
The following definitions are for handling cache alignment on the board.
MAX_CACHE_LINE must be set to the cache line size of the board. When allocating memory that must be cache aligned, it must be a multiple of the cache line size. Use board_roundup to get the appropriate size. As an example to allocate a cache aligned block of memory you would do something like: buffer_len_aligned = board_roundup (buffer_len, MAX_CACHE_LINE) Malloc (buffer_len_aligned)
#define board_roundup | ( | n, | |
w | |||
) | (((n) + (w) - 1) & ~((w) - 1)) |
#define BOARD_SOK 0 |
Board status OK
#define BOARD_INVALID_PARAM -1 |
Error code for invalid parameters
#define BOARD_UNSUPPORTED_FEATURE -2 |
Error code for unsupported feature
#define BOARD_I2C_OPEN_FAIL -3 |
I2C handle open failed
#define BOARD_I2C_TRANSFER_FAIL -4 |
I2C transfer call failed
#define BOARD_PINMUX_BAD_MEM_REGION -5 |
IO Delay region not in internal memory
#define BOARD_INIT_CLOCK_FAIL -6 |
Error code for init clock module
#define BOARD_INIT_DDR_FAIL -7 |
Error code for init DDR
#define BOARD_PINMUX_INVALID_MODE -8 |
Runtime pinmux configuration mode
#define BOARD_FAIL -10 |
Board status FAIL
#define BOARD_MAX_ID_STR_LEN 20 |
#define BOARD_BOARD_NAME_LEN (16U) |
#define BOARD_DESIGN_REV_LEN (2U) |
#define BOARD_PROC_NUM_LEN (4U) |
#define BOARD_VARIANT_LEN (2U) |
#define BOARD_PCBREV_LEN (2U) |
#define BOARD_SCHMBOM_REV_LEN (2U) |
#define BOARD_SWREV_LEN (2U) |
#define BOARD_VENDORID_LEN (2U) |
#define BOARD_BUILD_WEEK_LEN (2U) |
#define BOARD_BUILD_YEAR_LEN (2U) |
#define BOARD_BOARDID_LEN (6U) |
#define BOARD_SERIAL_NUM_LEN (4U) |
#define BOARD_MAC_ADDR_LEN (192U) |
#define BOARD_SYS_CLK_DEFAULT (0xFFFFFFFFU) |
#define BOARD_INIT_ALL (0xFFFFFFFFU) |
#define BOARD_INIT_UNLOCK_MMR (1 << 1U) |
#define BOARD_INIT_PLL (1 << 2U) |
#define BOARD_INIT_PLL_MCU (1 << 3U) |
#define BOARD_INIT_PLL_MAIN (1 << 4U) |
#define BOARD_INIT_MODULE_CLOCK (1 << 5U) |
#define BOARD_INIT_MODULE_CLOCK_MCU (1 << 6U) |
#define BOARD_INIT_MODULE_CLOCK_MAIN (1 << 7U) |
#define BOARD_INIT_DDR (1 << 8U) |
#define BOARD_INIT_WATCHDOG_DISABLE (1 << 9U) |
#define BOARD_INIT_PINMUX_CONFIG (1 << 10U) |
#define BOARD_INIT_PINMUX_CONFIG_MAIN (1 << 11U) |
#define BOARD_INIT_PINMUX_CONFIG_MCU (1 << 12U) |
#define BOARD_INIT_UART_STDIO (1 << 13U) |
#define BOARD_INIT_ICSS_PINMUX (1 << 14U) |
#define BOARD_INIT_ETH_PHY (1 << 15U) |
#define BOARD_INIT_ECC (1 << 16U) |
#define BOARD_INIT_PLL_OPP_HIGH (1 << 17U) |
#define BOARD_INIT_PLL_OPP_OD (1 << 18U) |
#define BOARD_INIT_PLL_OPP_NOM (1 << 19U) |
#define BOARD_INIT_ICSS_ETH_PHY (1 << 20U) |
#define BOARD_INIT_EMIF_PINMUX (1 << 21U) |
#define BOARD_INIT_DDR_ECC (1 << 22U) |
#define BOARD_INIT_SERDES_PHY (1 << 23U) |
#define BOARD_INIT_I2C (1 << 24U) |
#define BOARD_DEINIT_I2C (1 << 25U) |
#define BOARD_INIT_CPSW9G_ETH_PHY (1 << 26U) |
#define BOARD_INIT_ENETCTRL_CPSW3G (1 << 27U) |
#define BOARD_INIT_ENETCTRL_CPSW2G (1 << 27U) |
#define BOARD_INIT_ENETCTRL_CPSW9G (1 << 28U) |
#define BOARD_INIT_ENETCTRL_ICSS (1 << 29U) |
#define BOARD_INIT_DEFAULT BOARD_INIT_ALL |
#define BOARD_INIT_CPSW5G_ETH_PHY (BOARD_INIT_CPSW9G_ETH_PHY) |
#define BOARD_INIT_ENETCTRL_CPSW5G (BOARD_INIT_ENETCTRL_CPSW9G) |
#define BOARD_DEINIT_ALL (0xFFFFFFFFU) |
#define BOARD_DEINIT_LOCK_MMR (1 << 1U) |
#define BOARD_DEINIT_MODULE_CLOCK (1 << 2U) |
#define BOARD_DEINIT_UART_STDIO (1 << 3U) |
#define BOARD_DEINIT_DEFAULT BOARD_DEINIT_ALL |
#define BOARD_RESOURCE_ALL (0xFFFFU) |
#define BOARD_RESOURCE_MMR (1U) |
#define BOARD_RESOURCE_MODULE_CLOCK (2U) |
#define BOARD_RESOURCE_UART_STDIO (3U) |
#define BOARD_RESOURCE_SCICLIENT (4U) |
typedef uint32_t Board_initCfg |
typedef void(* Board_thermalMgmtCallbackFunction_t) (Board_DDRTempEventType DDRTempEventType) |
Enumeration of reported temperature event types.