PDK API Guide for J721E
|
This file contains the prototypes of the APIs present in the device abstraction layer file of CSI TX SS. This also contains some related macros.
Go to the source code of this file.
Data Structures | |
struct | CSL_CsitxRevisionId |
Structure for accessing Revision ID and Core Release Info. of CSI Tx module. More... | |
struct | CSL_CsitxColorbarGenCfg |
Structure for Color-bar generation configurations. More... | |
struct | CSL_CsitxRetransCfg |
Structure for re-transmission streams configurations. More... | |
struct | CSL_CsitxStrmStatus |
Structure for streams status. More... | |
struct | CSL_CsitxDMAConfig |
Structure for PSI-L/DMA configuration for CSI Tx SS. More... | |
Macros | |
#define | CSL_CSITX_PSI_L_THREAD_NUM_MAX ((uint32_t)32U) |
Maximum number of PSI-L Threads supported by CSI Tx SS. More... | |
CSITX DMA Data Size Shift | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS (0U) |
DMA Data Size Shift: 8 bits. More... | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS (1U) |
DMA Data Size Shift: 16 bits. More... | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS (2U) |
DMA Data Size Shift: 32 bits. More... | |
CSITX YUV422 Mode | |
#define | CSL_CSITX_YUV422_MODE_UYVY (0U) |
YUV422 Mode: UYVY. More... | |
#define | CSL_CSITX_YUV422_MODE_YUYV (2U) |
YUV422 Mode: VYUY. More... | |
#define | CSL_CSITX_YUV422_MODE_VYUY (1U) |
YUV422 Mode: YUYV. More... | |
#define | CSL_CSITX_YUV422_MODE_YVYU (3U) |
YUV422 Mode: YVYU. More... | |
Functions | |
void | CSL_csitxGetRevisionId (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxRevisionId *revId) |
This API is used get the CSI Tx revision ID. More... | |
int32_t | CSL_csitxColorbarCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxColorbarGenCfg *cfg) |
This API is used program the color bar generation parameters. More... | |
void | CSL_csitxEnableColorbarGen (CSL_csi_tx_ifRegs *ifRegisters, uint32_t enable) |
This API is used enable/disable Color-bar generation. More... | |
int32_t | CSL_csitxRetransCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxRetransCfg *cfg) |
This API is used program the re-transmission streams parameters. More... | |
void | CSL_csitxAssertPixelIfReset (CSL_csi_tx_ifRegs *ifRegisters, uint32_t assert) |
This API is used assert/de-assert reset for pixel interface. More... | |
void | CSL_csitxGetStrmStatus (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxStrmStatus *status) |
This API is used get the current stream status. More... | |
int32_t | CSL_csitxFrmToFrmDelayCfg (const CSL_csi_tx_ifRegs *ifRegisters, const uint32_t vc, const uint32_t delay) |
This API is used program frame to frame delay. More... | |
int32_t | CSL_csitxConfigDMA (CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxDMAConfig *cfg) |
This API is used to configure DMA/PSIL thread. More... | |