|
PDK API Guide for J721E
|
Go to the documentation of this file. 71 #define CSIRX_NUM_CH (CSIRX_NUM_CH_MAX) 73 #define CSIRX_CH_ID_DEFAULT ((uint32_t) 0x00U) 76 #define CSIRX_VC_NUM_DEFAULT ((uint32_t) 0x00U) 78 #define CSIRX_IN_DT_DEFAULT (FVID2_CSI2_DF_RGB888) 81 #define CSIRX_CAPT_QUEUE_DEPTH_PER_CH ((uint32_t)10U) 83 #define CSIRX_TIMEOUT_VAL_MS ((uint32_t)10U) 87 #define CsirxTrace ((uint32_t) GT_INFO |\ 88 (uint32_t) GT_TraceState_Enable) 92 #define CSIRX_DRV_ENABLE_DEBUG (0U) 94 #define CSIRX_DRV_LOG_CNT (2000U)