MCUSW
Wdg_Cfg.h File Reference

Introduction

This file contains generated pre compile configuration file for WDG MCAL driver.

Go to the source code of this file.

Macros

#define WDG_VARIANT_PRE_COMPILE   (STD_ON)
 WDG Build Variant. Build variants.(i.e Pre Compile,Link Time And Post Build) More...
 
#define WDG_INIT_CONFIG_PC   WdgSettingsConfig
 Pre Compile config macro name. More...
 
#define WDG_DEV_ERROR_DETECT   (STD_ON)
 Enable/Disable Development Error Detection. More...
 
#define WDG_GET_VERSION_INFO_API   (STD_ON)
 Enable/Disable Version Info API. More...
 
#define WDG_REGISTER_READBACK_API   (STD_ON)
 Enable/Disable Register Readback API. More...
 
#define WDG_MAX_TIMEOUT   ((uint16)65535)
 Watchdog Maximum Timeout x 1000U - converting from secs so milli secs. More...
 
#define WDG_RTI_FREQUENCY   ((uint32)12500000)
 RTI Clock Frequency. More...
 
#define WDG_DISABLE_ALLOWED   (STD_OFF)
 Watchdog Disable Allowed. More...
 
WDG Module Instance Id

Symbolic names for module instance id

#define WdgConf_WdgGeneral_WdgIndex_0   (0U)
 Wdg Module Instance Id, always 0 as only one instance in this case. More...
 
WDG DEM Error codes to report

Pre-compile switches for enabling/disabling DEM events

#define DemConf_DemEventParameter_WDG_DEM_NO_EVENT   (0xFFFFU)
 
#define WDG_DEM_NO_EVENT   DemConf_DemEventParameter_WDG_DEM_NO_EVENT
 
#define WDG_E_MODE_FAILED   DemConf_DemEventParameter_WDG_E_MODE_FAILED
 Mode failed. More...
 
#define WDG_E_DISABLE_REJECTED   DemConf_DemEventParameter_WDG_E_DISABLE_REJECTED
 Disabled rejected. More...
 

Variables

const struct Wdg_ConfigType_s WdgSettingsConfig
 WDG Configuration struct declaration. More...
 
const struct Wdg_ConfigType_PC_s WdgSettingsConfig_PC
 WDG Configuration pre compile struct declaration. More...