MCUSW
|
This file contains generated pre compile configuration file for SPI MCAL driver.
Go to the source code of this file.
Macros | |
#define | SPI_VARIANT_POST_BUILD (STD_ON) |
SPI Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time) More... | |
#define | SPI_CHANNELBUFFERS (SPI_IB_EB) |
Pre Compile config macro name. More... | |
#define | SPI_IB_MAX_LENGTH (64U) |
Internal Buffer length in bytes - applicable only for SPI_IB. More... | |
#define | SPI_DEV_ERROR_DETECT (STD_ON) |
Enable/disable SPI dev detect error. More... | |
#define | SPI_JOB_LOG (STD_ON) |
Enable/disable SPI job log. More... | |
#define | SPI_MAX_JOB_LOG (100U) |
Maximum job log entries when logging is ON. More... | |
#define | SPI_MAX_HW_DMA_UNIT (0U) |
Enable/disable SPI DMA Support. More... | |
#define | SPI_DMA_ENABLE (STD_OFF) |
Enable/disable SPI DMA Support. More... | |
#define | SPI_LEVEL_0 (0U) |
Basic Synchronous functions. More... | |
#define | SPI_LEVEL_1 (1U) |
Basic Asynchronous functions. More... | |
#define | SPI_LEVEL_2 (2U) |
Synchronous and Asynchronous functions. More... | |
#define | SPI_SUPPORT_CONCURRENT_SYNC_TRANSMIT (STD_OFF) |
Concurrent sync transmit support - by defualt this is off. More... | |
#define | SPI_SCALEABILITY (SPI_LEVEL_2) |
Scalability level. More... | |
#define | SPI_VERSION_INFO_API (STD_ON) |
Enable/disable SPI get version info API. More... | |
#define | SPI_HW_STATUS_API (STD_ON) |
Enable/disable SPI HW Status API. More... | |
#define | SPI_CANCEL_API (STD_ON) |
Enable/disable SPI cancel API. More... | |
#define | SPI_MAX_CHANNELS_PER_JOB (1U) |
Maximum channels allowed per job. More... | |
#define | SPI_MAX_JOBS_PER_SEQ (1U) |
Maximum jobs allowed per sequence. More... | |
#define | SPI_MAX_CHANNELS (1U) |
Maximum channels across all jobs/sequence/hwunit. More... | |
#define | SPI_MAX_JOBS (1U) |
Maximum jobs across all sequence/hwunit. More... | |
#define | SPI_MAX_SEQ (1U) |
Maximum sequence across all hwunit. More... | |
#define | SPI_MAX_HW_UNIT (8U) |
Maximum HW unit - This should match the sum for the below units ISR which are ON. More... | |
#define | SPI_MAX_EXT_DEV (11U) |
Maximum external device cfg. More... | |
#define | SPI_UNIT_MCU_MCSPI0_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI0 unit ISR. More... | |
#define | SPI_UNIT_MCU_MCSPI1_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI1 unit ISR. More... | |
#define | SPI_UNIT_MCU_MCSPI2_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI2 unit ISR. More... | |
#define | SPI_UNIT_MCSPI0_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI0 unit ISR. More... | |
#define | SPI_UNIT_MCSPI1_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI1 unit ISR. More... | |
#define | SPI_UNIT_MCSPI2_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI2 unit ISR. More... | |
#define | SPI_UNIT_MCSPI3_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI3 unit ISR. More... | |
#define | SPI_UNIT_MCSPI4_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI4 unit ISR. More... | |
#define | SPI_UNIT_MCSPI5_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI5 unit ISR. More... | |
#define | SPI_UNIT_MCSPI6_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI6 unit ISR. More... | |
#define | SPI_UNIT_MCSPI7_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI7 unit ISR. More... | |
#define | SPI_ISR_TYPE (SPI_ISR_CAT1) |
ISR type. More... | |
#define | SPI_OS_COUNTER_ID ((CounterType)OsCounter_0) |
OS counter ID - used for timeout in case of error. More... | |
#define | SPI_TIMEOUT_DURATION (32000U) |
SPI timeout - used in McSPI IP reset Each tick is 31.25us (for 32K Counter). Wait for 100ms which comes to below value. More... | |
#define | SPI_REGISTER_READBACK_API (STD_ON) |
Enable/disable SPI register read back API. More... | |
#define | SpiConf_SpiChannel_SpiChannel_0 (0U) |
Symbolic Name Channel Id - 0 SpiChannel_0. More... | |
#define | SpiConf_SpiExternalDevice_CS0 (SPI_CS0) |
Symbolic Name Chip Select - 0. More... | |
#define | SpiConf_SpiJob_SpiJob_0 (0U) |
Symbolic Name Job Id - 0 SpiJob_0. More... | |
#define | SpiConf_SpiSequence_SpiSequence_0 (0U) |
Symbolic Name Sequence Id - 0 SpiSequence_0. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId0 (CSIB0) |
Symbolic Name HW Unit - 0. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId1 (CSIB1) |
Symbolic Name HW Unit - 1. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId2 (CSIB2) |
Symbolic Name HW Unit - 2. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId3 (CSIB3) |
Symbolic Name HW Unit - 3. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId4 (CSIB4) |
Symbolic Name HW Unit - 4. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId5 (CSIB5) |
Symbolic Name HW Unit - 5. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId6 (CSIB6) |
Symbolic Name HW Unit - 6. More... | |
#define | SpiConf_SpiExternalDevice_HwUnitId7 (CSIB7) |
Symbolic Name HW Unit - 7. More... | |
SPI DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
#define | DemConf_DemEventParameter_SPI_DEM_NO_EVENT (0xFFFFU) |
#define | SPI_DEM_NO_EVENT DemConf_DemEventParameter_SPI_DEM_NO_EVENT |
#define | SPI_E_HARDWARE_ERROR (DemConf_DemEventParameter_SPI_E_HARDWARE_ERROR) |
Hardware failed. More... | |
Functions | |
void | SpiApp_wbInvCache (uint8 *buf, uint16 len) |
Cache write-back invalidate function. More... | |
void | SpiApp_wbCache (uint8 *buf, uint16 len) |
Cache write-back function. More... | |
void | SpiApp_invCache (uint8 *buf, uint16 len) |
Cache invalidate function. More... | |
Variables | |
const struct Spi_ConfigType_s | SpiDriver |
SPI Configuration struct declaration. More... | |