MCUSW
|
This file contains generated pre compile configurations for GPT MCAL driver.
Go to the source code of this file.
Macros | |
#define | GPT_PRE_COMPILE_VARIANT (STD_OFF) |
GPT Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild. More... | |
#define | GPT_DEV_ERROR_DETECT (STD_ON) |
Enable/disable GPT dev detect error. More... | |
#define | GPT_ISR_TYPE (GPT_ISR_CAT1) |
ISR type. More... | |
#define | GPT_REPORT_WAKEUP_SOURCE (STD_ON) |
Enable/disable wakeup source in wakeup related APIs. More... | |
#define | GPT_MAX_CHANNELS (5U) |
No. of channels configured for GPT driver. More... | |
#define | GPT_PREDEF_TIMER_TYPE (GPT_PREDEF_TIMER_DISABLED) |
Macro for enabling predefined timers This is in case to disable GPT Predef Timers if timers can not be supported by hardware reasons. More... | |
#define | GPT_PREDEF_TIMER_1US_ENABLING_GRADE (GPT_PREDEF_TIMER_1US_DISABLED) |
: Specifies the grade of enabling the GPT Predef Timers with 1us tick duration More... | |
#define | GPT_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks. More... | |
#define | GPT_TIMEOUT_DURATION (32000U) |
ETH timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value. More... | |
#define | GPT_REGISTER_READBACK_API (STD_ON) |
Enable/disable GPT register read back API. More... | |
#define | GptConf_GptChannelConfiguration_TIMER1 (11U) |
Channel ID Configured channel ID(s) More... | |
#define | GptConf_GptChannelConfiguration_MCU_TIMER6 (6U) |
#define | GptConf_GptChannelConfiguration_MCU_TIMER9 (9U) |
#define | GptConf_GptChannelConfiguration_TIMER5 (15U) |
#define | GptConf_GptChannelConfiguration_TIMER19 (29U) |
Pre-Compile Switches for API Services | |
#define | GPT_VERSION_INFO_API (STD_ON) |
Enable/disable GPT get version info API. More... | |
#define | GPT_DEINIT_API (STD_ON) |
Enable/disable GPT deinit API. More... | |
#define | GPT_TIME_ELAPSED_API (STD_ON) |
Enable/disable GPT get time elapsed API. More... | |
#define | GPT_TIME_REMAINING_API (STD_ON) |
Enable/disable GPT time remaining API. More... | |
#define | GPT_ENABLE_DISABLE_NOTIFICATION_API (STD_ON) |
Enable/disable GPT enable/disable GPT API. More... | |
#define | GPT_WAKEUP_FUNCTIONALITY_API (STD_ON) |
Enable/disable GPT wakeup functionality API. More... | |
GPT DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
#define | DemConf_DemEventParameter_GPT_DEM_NO_EVENT (0xFFFFU) |
#define | GPT_DEM_NO_EVENT DemConf_DemEventParameter_GPT_DEM_NO_EVENT |
#define | GPT_E_HARDWARE_ERROR (DemConf_DemEventParameter_GPT_E_HARDWARE_ERROR) |
Hardware failed. More... | |
Variables | |
const struct Gpt_ConfigType_s | GptChannelConfigSet |
GPT Configuration. More... | |