MCUSW
|
This file contains interface header for Ethernet Transceiver MCAL driver.
Go to the source code of this file.
Macros | |
EthTrcv Driver Module SW Version Info | |
Defines for ETHTRCV Driver version used for compatibility checks | |
#define | ETHTRCV_SW_MAJOR_VERSION (1U) |
Driver Implementation Major Version. More... | |
#define | ETHTRCV_SW_MINOR_VERSION (3U) |
Driver Implementation Minor Version. More... | |
#define | ETHTRCV_SW_PATCH_VERSION (4U) |
Driver Implementation Patch Version. More... | |
EthTrcv Driver Module AUTOSAR Version Info | |
Defines for ETHTRCV Driver AUTOSAR version used for compatibility checks | |
#define | ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major Version implemented. More... | |
#define | ETHTRCV_AR_RELEASE_MINOR_VERSION (2U) |
AUTOSAR Minor Version implemented. More... | |
#define | ETHTRCV_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR patch Version implemented. More... | |
EthTrcv Driver ID Info | |
#define | ETHTRCV_VENDOR_ID (44U) |
Texas Instruments Vendor ID. More... | |
#define | ETHTRCV_MODULE_ID (73U) |
EthTrcv Driver ID. More... | |
#define | ETHTRCV_INSTANCE_ID (0U) |
EthTrcv Instace ID. More... | |
EthTrcv Driver Service Id | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
#define | ETHTRCV_INIT_ID ((uint8) 0x01U) |
EthTrcv_Init() API Service ID. More... | |
#define | ETHTRCV_SETTRCVMODE_ID ((uint8) 0x03U) |
EthTrcv_SetTransceiverMode() API Service ID. More... | |
#define | ETHTRCV_GETTRCVMODE_ID ((uint8) 0x04U) |
EthTrcv_GetTransceiverMode() API Service ID. More... | |
#define | ETHTRCV_SRTAUTONEGOTIA_ID ((uint8) 0x05U) |
EthTrcv_StartAutoNegotiation() API Service ID. More... | |
#define | ETHTRCV_GETLNKSTATE_ID ((uint8) 0x06U) |
EthTrcv_GetLinkState() API Service ID. More... | |
#define | ETHTRCV_GETBAUD_ID ((uint8) 0x07U) |
EthTrcv_GetBaudRate() API Service ID. More... | |
#define | ETHTRCV_GETDPLXMODE_ID ((uint8) 0x08U) |
EthTrcv_GetDuplexMode() API Service ID. More... | |
#define | ETHTRCV_READMIIIND_ID ((uint8) 0x09U) |
EthTrcv_ReadMiiIndication callback() API Service ID. More... | |
#define | ETHTRCV_WRITEMIIIND_ID ((uint8) 0x0AU) |
EthTrcv_WriteMiiIndication callback() API Service ID. More... | |
#define | ETHTRCV_VERSION_ID ((uint8) 0x0BU) |
EthTrcv_GetVersionInfo() API Service ID. More... | |
#define | ETHTRCV_MAINFCT_WRITE_ID ((uint8) 0x0CU) |
EthTrcv_MainFunction() API Service ID. More... | |
#define | ETHTRCV_GETTRCVWKUPMODE_ID ((uint8) 0x0DU) |
EthTrcv_GetTransceiverWakeupMode() API Service ID. More... | |
#define | ETHTRCV_SETTRCVWKUPMODE_ID ((uint8) 0x0EU) |
EthTrcv_SetTransceiverWakeupMode() API Service ID. More... | |
#define | ETHTRCV_CHKWKUP_ID ((uint8) 0x0FU) |
EthTrcv_CheckWakeup() API Service ID. More... | |
#define | ETHTRCV_SETPHYTESTMODE_ID ((uint8) 0x10U) |
EthTrcv_SetPhyTestMode() API Service ID. More... | |
#define | ETHTRCV_SETPHYLOOPBACKMODE_ID ((uint8) 0x11U) |
EthTrcv_SetPhyLoopbackMode() API Service ID. More... | |
#define | ETHTRCV_GETPHYSIGNALQUALITY_ID ((uint8) 0x12U) |
EthTrcv_GetPhySignalQuality() API Service ID. More... | |
#define | ETHTRCV_SETPHYTXMODE_ID ((uint8) 0x13U) |
EthTrcv_SetPhyTxMode() API Service ID. More... | |
#define | ETHTRCV_GETCABLEDIAGNOSTICSRESULT_ID ((uint8) 0x014U) |
EthTrcv_GetCableDiagnosticsResult() API Service ID. More... | |
#define | ETHTRCV_GETPHYIDENTIFIER_ID ((uint8) 0x015U) |
EthTrcv_GetPhyIdentifier() API Service ID. More... | |
EthTrcv Error Codes | |
Error codes returned by EthTrcv functions | |
#define | ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U) |
Invalid transceiver index. More... | |
#define | ETHTRCV_E_UNINIT ((uint8) 0x02U) |
EthTrcv module was not initialized. More... | |
#define | ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U) |
#define | ETHTRCV_E_INIT_FAILED ((uint8) 0x04U) |
EthTrcv Wake-up Modes | |
Ethernet Transceiver wakeup support definitions used to configure wake-up to polling or interrupt or to not used/not supported. | |
#define | ETHTRCV_WAKEUP_BY_INTERRUPT (0x0U) |
Interrupt based wake up for Ethernet Transceiver. More... | |
#define | ETHTRCV_WAKEUP_BY_POLLING (0x1U) |
Polling based wake up for Ethernet Transceiver. More... | |
#define | ETHTRCV_WAKEUP_NOT_SUPPORTED (0x2U) |
Wake up for Ethernet Transceiver not supported. More... | |
Functions | |
void | EthTrcv_Init (const EthTrcv_ConfigType *CfgPtr) |
This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function. More... | |
Std_ReturnType | EthTrcv_SetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType CtrlMode) |
This function enables / disables the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_GetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType *TrcvModePtr) |
This function obtains the state of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_SetTransceiverWakeupMode (uint8 TrcvIdx, EthTrcv_WakeupModeType TrcvWakeupMode) |
This function enables / disables the wake-up mode or clear the wake-up reason of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_GetTransceiverWakeupMode (uint8 TrcvIdx, EthTrcv_WakeupModeType *TrcvWakeupModePtr) |
This function returns the wake up mode of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_CheckWakeup (uint8 TrcvIdx) |
This service is called by EthIf in case a wake-up interrupt is detected. More... | |
Std_ReturnType | EthTrcv_StartAutoNegotiation (uint8 TrcvIdx) |
This function restarts the negotiation of the transmission parameters used by the indexed. More... | |
Std_ReturnType | EthTrcv_GetLinkState (uint8 TrcvIdx, EthTrcv_LinkStateType *LinkStatePtr) |
This function obtains the link state of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_GetBaudRate (uint8 TrcvIdx, EthTrcv_BaudRateType *BaudRatePtr) |
This function obtains the baud rate of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_GetDuplexMode (uint8 TrcvIdx, EthTrcv_DuplexModeType *DuplexModePtr) |
This function obtains the duplex mode of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_SetPhyTestMode (uint8 TrcvIdx, EthTrcv_PhyTestModeType Mode) |
This function Activates a given test mode. More... | |
Std_ReturnType | EthTrcv_SetPhyLoopbackMode (uint8 TrcvIdx, EthTrcv_PhyLoopbackModeType Mode) |
This function Activates a given loopback mode. More... | |
Std_ReturnType | EthTrcv_GetPhySignalQuality (uint8 TrcvIdx, uint32 *SignalQualityPtr) |
This function Obtains the current signal quality of the link of the indexed transceiver. More... | |
Std_ReturnType | EthTrcv_SetPhyTxMode (uint8 TrcvIdx, EthTrcv_PhyTxModeType Mode) |
This function Activates a given transmission mode. More... | |
Std_ReturnType | EthTrcv_GetCableDiagnosticsResult (uint8 TrcvIdx, EthTrcv_CableDiagResultType *ResultPtr) |
This function Retrieves the cable diagnostics result of a given transceiver. More... | |
Std_ReturnType Std_ReturnType | EthTrcv_GetPhyIdentifier (uint8 TrcvIdx, uint32 *OrgUniqueIdPtr, uint8 *ModelNrPtr, uint8 *RevisionNrPtr) |
This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802.3-2015 chapter 22.2.4.3.1 PHY Identifer. More... | |
void | EthTrcv_GetVersionInfo (Std_VersionInfoType *VersionInfoPtr) |
Function returns the version information of this module. More... | |
void | EthTrcv_ReadMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal) |
This function is called when information has been read out via MII interface. Triggered by previous Eth_ReadMii call. It can directly be called within Eth_ReadMii. More... | |
void | EthTrcv_WriteMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegId) |
This function is called when information has been written via MII interface. Triggered by previous Eth_WriteMii call. It can directly be called within Eth_WriteMii. More... | |
void | EthTrcv_MainFunction (void) |
This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication when the transceiver mode changed. It stores wakeup events if EthTrcvWakeUpSupport is set to ETHTRCV_WAKEUP_BY_POLLING. More... | |