Atanhsp


Detailed Description


Functions

float atanhsp_c (float a)
float atanhsp (float a)


Function Documentation

float atanhsp_c ( float  a  ) 

Description:
The atanhsp function returns the inverse hyperbolic tanget function of a real floating-point argument a. The input must be within the range [-1, 1].
Parameters:
[in] a = Input float
Returns:
Resultant float
Special Cases:
  • If a is not within the range [-1, 1], the return value is NaN (Not a Number).
  • If |a| = 1, the return value is is INF (infinity).
  • If a is NaN (Not a Number), the return value is NaN.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

float atanhsp ( float  a  ) 


Copyright 2016, Texas Instruments Incorporated