Asinhdp


Detailed Description


Functions

double asinhdp_c (double a)
double asinhdp (double a)


Function Documentation

double asinhdp_c ( double  a  ) 

Description:
The asinhdp function returns the inverse hyperbolic sine function of a real floating-point argument a.
Parameters:
[in] a = Input double
Returns:
Resultant double
Special Cases:

See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double asinhdp ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated