EthFw Release Notes

Version: 08.02.00.03

Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. What's New
  6. Upgrade and Compatibility Information
  7. Device Support
  8. Validation Information
  9. Fixed Issues
  10. Known Issues
  11. Dependencies
  12. Technical Support
  13. Package Versioning


Introduction

This release notes provides important information that will assist you in using the EthFw component. This document provides the product information and known issues with respect to EthFw software component. The EthFw component consists of firmware for Ethernet switch, profiling tools and demos/applications for J721E and J7200 silicon platforms.

Licensing

Refer to Processor SDK RTOS top-level manifest.

Getting Started

The Ethernet Firmware User's Guide provides the documentation and references necessary to run EthFw demos and begin development on TI's platforms.

Documentation

Refer to following documentation for further details:

Ethernet Firmware User Guide Build instructions, Demos [HTML]
Ethernet Firmware API Guide API Guide [HTML]

What's New

Upgrade and Compatibility Information

None for this release.

Device Support

Below table shows device support for EthFw.
SoC HOST (OS) Target (OS) Test Platform
J721E Linux FreeRTOS J721E EVM with GESI and QSGMII Daughter Boards
J7200 Linux FreeRTOS J7200 EVM with QSGMII Daughter Board

Refer Processor SDK RTOS RTOS release notes for SDK device support.

Validation Information

This release was built and validated using the following tools. Refer to the EthFw User's Guide for additional instructions to install and setup the dependencies.

Build Tools (included in Processor SDK)

Fixed Issues

Issue ID Headline Module Affected Platforms Reported in Release Fixed in Release
ETHFW-607 EthFw - QSGMII daughter board not supported with Linux EthFw J721E 06.02.00.04 08.02.00.00
ETHFW-1733 demo: Rate limiting demo exceeded intended rate in egress port EthFw J721E, J7200 07.00.00.00 08.02.00.00
ETHFW-1902 EthFw: ARP request fails in Linux virtual MAC (switch port) with static IP EthFw J721E, J7200 08.01.00.00 08.02.00.00
ETHFW-1904 Enet: High packet drop in iperf UDP test Enet LLD J721E, J7200 08.01.00.00 08.02.00.00
ETHFW-1924 timeSync: cpsw: ALE policer rate limiting fields not initialized TimeSync / PTP J721E, J7200 07.00.00.00 08.02.00.00
ETHFW-1925 timesync: Reset due to missed SYNC frames TimeSync / PTP J721E, J7200 07.00.00.00 08.02.00.00
ETHFW-1926 timesync: CPSW: Incorrect timestamp adjustment direction TimeSync / PTP J721E, J7200 07.00.00.00 08.02.00.00

Known Issues and Limitations

Issue ID Head Line Module Reported in Release Affected Platforms Workaround in this release
PROC_BRDS-658 MAC PORT 0 packet drop seen of Rx/TX - Packet drop is seen on MAC PORT0 (RGMII1) on 1Gbps mode on GESI board of J721E EVM alpha version. This port is labeled as PRG1_RGMII1_B in the GESI board connections figure in @ref ethfw_depend_evm_gesi_j721e section.
This issue is not applicable to J721E EVM beta version
Alpha EVM 00.08.00.00 J721E Reduce MAC port 0 speed to 100Mbps in J721E EVM alpha version.
PROC_BRDS-671 External 50MHz RMII clock from PHY is not connected by default to SoC's RMII_REF_CLOCK pin in GESI boards of J721E EVM alpha version
This issue is not applicable to J721E EVM beta version
Alpha EVM 00.08.00.00 J721E To get RMII_50MHZ_CLK, resistor R225 needs to be populated. Move R226 to R225 on GESI board to get this clock.
PROC_BRDS-659 QSGMII expansion board is causing instabilities in the MDIO bus in J721E EVM alpha version. After a few mins, MDIO register access fail.
This issue is not applicable to J721E EVM beta version.
Alpha EVM 00.08.00.00 J721E Disconnect QUAD PORT ETH expansion board from Alpha EVM.
ETHFW-607 EthFw - QSGMII daughter board not supported with Linux EthFw 06.02.00.04 J721E QSGMII daugther board is not supported in Linux due to SERDES sharing not enabled. In order to use QSGMII ports, SERDES usage from Linux has to be disabled. Contact TI representative for detailed instructions to enable QSGMII ports.
ETHFW-1733 demo: Rate limiting demo exceeded intended rate in egress port EthFw 07.00.00.00 J721E, J7200 When sending packets at a rate higher than programmed in the demo (200Mbps), for instance 250Mbps, the egress port should see its rate limited to 200Mbps. But the rate at egress port is same as the ingress port.
ETHFW-1902 EthFw: ARP request fails in Linux virtual MAC (switch port) with static IP EthFw 08.01.00.00 J721E, J7200 Replace default firmware in Linux with precompiled images from EthFw component directory.

Dependencies

All Ethernet Firmware dependencies are also part of the SDK, please refer to the User's Guide for details.

Technical Support

For technical support and additional assistance, contact local TI Field Application Engineer

Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p.

Copyright 2021, Texas Instruments Incorporated