Struct containing config parameters of given static value.
More...
#include <tivx.h>
Struct containing config parameters of given static value.
Definition at line 145 of file tivx.h.
◆ max_value
uint32_t tivx_resource_stats_t::max_value |
< Maximum value of a macro Value currently being used by a statically allocated array
Definition at line 148 of file tivx.h.
◆ cur_used_value
uint32_t tivx_resource_stats_t::cur_used_value |
Highest value used at any point of the application
Definition at line 151 of file tivx.h.
◆ max_used_value
uint32_t tivx_resource_stats_t::max_used_value |
Name of the macro
Definition at line 154 of file tivx.h.
The documentation for this struct was generated from the following file: