![]() |
TIOVX User Guide
|
distribution object descriptor as placed in shared memory More...
#include <tivx_obj_desc.h>
Data Fields | |
tivx_obj_desc_t | base |
base object descriptor | |
tivx_shared_mem_ptr_t | mem_ptr |
distribution memory address | |
volatile uint32_t | num_bins |
number of rows | |
volatile uint32_t | offset |
number of columns | |
volatile uint32_t | range |
scale factor | |
volatile uint32_t | num_win |
number of windows | |
volatile uint32_t | mem_size |
size of buffer pointed to by mem_ptr | |
distribution object descriptor as placed in shared memory
Definition at line 686 of file tivx_obj_desc.h.