![]() |
TIOVX User Guide
|
Internal APIs for utility operations.
Defines | |
#define | TIVX_ALIGN(value, align) ((((value)+((align)-1U))/(align))*(align)) |
Macro to align a 'value' to 'align' units. | |
#define | TIVX_FLOOR(value, align) (((value)/(align))*(align)) |
Macro to floor a 'value' to 'align' units. | |
#define | TIVX_DEFAULT_STRIDE_Y_ALIGN (64U) |
Macro to specify default alignment to use for stride in Y-direction. More... | |
#define | TIVX_TYPE_IS_SCALAR(type) (((vx_enum)VX_TYPE_INVALID < (type)) && ((type) < (vx_enum)VX_TYPE_SCALAR_MAX)) |
Used to determine if a type is a scalar. | |
#define | TIVX_TYPE_IS_STRUCT(type) (((type) >= (vx_enum)VX_TYPE_RECTANGLE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_STRUCT_MAX)) |
Used to determine if a type is a struct. | |
#define | TIVX_TYPE_IS_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_REFERENCE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_OBJECT_END)) |
Used to determine if a type is an Khronos defined object. | |
#define | TIVX_TYPE_IS_TI_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_VENDOR_OBJECT_START) && ((type) < (vx_enum)VX_TYPE_VENDOR_OBJECT_END)) |
Used to determine if a type is TI defined object. | |
#define | TIVX_MAGIC (0xFACEC0DEU) |
A magic value to look for and set in references. | |
#define | TIVX_BAD_MAGIC (42U) |
A magic value to look for and set in references. Used to indicate a free'ed reference. | |
#define | VX_CHECK_PARAM(ptr, size, type, align) ((size == sizeof(type)) && (((vx_size)ptr & align) == 0U)) |
A parameter checker for size and alignment. | |
Enumerations | |
enum | tivx_type_e |
TIVX defined reference types. | |
Functions | |
static void | tivx_uint32_to_uint64 (volatile uint64_t *val, uint32_t h, uint32_t l) |
Macro to convert 2x uint32 to uint64. | |
static void | tivx_uint64_to_uint32 (uint64_t val, volatile uint32_t *h, volatile uint32_t *l) |
Macro to convert uint64 to 2x uint32. | |
#define TIVX_DEFAULT_STRIDE_Y_ALIGN (64U) |
Macro to specify default alignment to use for stride in Y-direction.
Video codecs require 64 byte alignment Remaining HWA nodes require 16 byte alignment
Definition at line 118 of file vx_internal.h.