![]() |
TIOVX User Guide
|
APIs for kernel operations on the target.
Typedefs | |
typedef struct _tivx_target_kernel * | tivx_target_kernel |
Handle to kernel on a target. | |
typedef struct _tivx_target_kernel_instance * | tivx_target_kernel_instance |
Handle to instance of kernel on a target. | |
typedef vx_status(VX_CALLBACK * | tivx_target_kernel_f) (tivx_target_kernel_instance kernel, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback. More... | |
typedef vx_status(VX_CALLBACK * | tivx_target_kernel_control_f) (tivx_target_kernel_instance kernel, uint32_t node_cmd_id, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback for control command. More... | |
Functions | |
VX_API_ENTRY tivx_target_kernel VX_API_CALL | tivxAddTargetKernel (vx_enum kernel_id, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg) |
Allows users to add native kernels implementation to specific targets. More... | |
VX_API_ENTRY tivx_target_kernel VX_API_CALL | tivxAddTargetKernelByName (const char *kernel_name, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg) |
Allows users to add native kernels implementation to specific targets. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxRemoveTargetKernel (tivx_target_kernel target_kernel) |
Allows users to remove native kernels implementation to specific targets. | |
VX_API_ENTRY vx_status VX_API_CALL | tivxSetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void *kernel_context, uint32_t kernel_context_size) |
Associate a kernel function context or handle with a target kernel instance. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxGetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void **kernel_context, uint32_t *kernel_context_size) |
Get a kernel function context or handle with a target kernel instance. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxGetTargetKernelInstanceState (tivx_target_kernel_instance target_kernel_instance, vx_enum *state) |
Get a kernel state with a target kernel instance. More... | |
VX_API_ENTRY void | tivxGetTargetKernelInstanceBorderMode (tivx_target_kernel_instance target_kernel_instance, vx_border_t *border_mode) |
Get the border mode for the target kernel instance. More... | |
VX_API_ENTRY vx_bool | tivxIsTargetKernelInstanceReplicated (tivx_target_kernel_instance kernel_instance) |
Checks if supplied node is replicated. Returns vx_true if the given node is replicated and vx_false if not. | |
typedef vx_status(VX_CALLBACK * tivx_target_kernel_f) (tivx_target_kernel_instance kernel, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback.
For create_func, delete_func and process_func callbacks 'obj_desc' points to array of data object descriptor parameters For control_func, 'obj_desc' points to array of objects descriptors where obj_desc[0] points to the node object descriptors obj_desc[1..num_params-1] points to target kernel defined parameters
[in] | kernel | The kernel for which the callback is called |
[in] | obj_desc | Object descriptor passed as input to this callback |
Definition at line 107 of file tivx_target_kernel.h.
typedef vx_status(VX_CALLBACK * tivx_target_kernel_control_f) (tivx_target_kernel_instance kernel, uint32_t node_cmd_id, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback for control command.
For create_func, delete_func and process_func callbacks 'obj_desc' points to array of data object descriptor parameters For control_func, 'obj_desc' points to array of objects descriptors for control parameter. It could be any vx_(object)
[in] | kernel | The kernel for which the callback is called |
[in] | Command | ID to be processed in the given node |
[in] | obj_desc | Object descriptor passed as input to this callback |
[in] | num_params | valid entries in object descriptor (obj_desc) array |
Definition at line 127 of file tivx_target_kernel.h.
VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernel | ( | vx_enum | kernel_id, |
const char * | target_name, | ||
tivx_target_kernel_f | process_func, | ||
tivx_target_kernel_f | create_func, | ||
tivx_target_kernel_f | delete_func, | ||
tivx_target_kernel_control_f | control_func, | ||
void * | priv_arg | ||
) |
Allows users to add native kernels implementation to specific targets.
This is different from vxAddUserKernel() in that this is called on the target CPU. This is a TI prorietary API and not part of OpenVX or TI OpenVX extention. This allows users to implement and plugin specific target optimized kernels on TI platforms A equivalent vxAddUserKernel is typically called to pair the target kernel with OpenVX user kernel.
VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernelByName | ( | const char * | kernel_name, |
const char * | target_name, | ||
tivx_target_kernel_f | process_func, | ||
tivx_target_kernel_f | create_func, | ||
tivx_target_kernel_f | delete_func, | ||
tivx_target_kernel_control_f | control_func, | ||
void * | priv_arg | ||
) |
Allows users to add native kernels implementation to specific targets.
Same as tivxAddTargetKernel except that it take a string name as input instead of kernel_id
VX_API_ENTRY vx_status VX_API_CALL tivxSetTargetKernelInstanceContext | ( | tivx_target_kernel_instance | target_kernel_instance, |
void * | kernel_context, | ||
uint32_t | kernel_context_size | ||
) |
Associate a kernel function context or handle with a target kernel instance.
Typically set by the kernel function during create phase
VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceContext | ( | tivx_target_kernel_instance | target_kernel_instance, |
void ** | kernel_context, | ||
uint32_t * | kernel_context_size | ||
) |
Get a kernel function context or handle with a target kernel instance.
Typically used by the kernel function during run, control, delete phase
VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceState | ( | tivx_target_kernel_instance | target_kernel_instance, |
vx_enum * | state | ||
) |
Get a kernel state with a target kernel instance.
Typically used by a capture kernel function during process to track state
VX_API_ENTRY void tivxGetTargetKernelInstanceBorderMode | ( | tivx_target_kernel_instance | target_kernel_instance, |
vx_border_t * | border_mode | ||
) |
Get the border mode for the target kernel instance.
Used by the kernel implemention to get border mode