![]() |
TIOVX User Guide
|
Internal APIs for object descriptor operations.
Data Structures | |
| struct | tivx_obj_desc_cmd_t |
| Command object descriptor. More... | |
| struct | tivx_obj_desc_kernel_name_t |
| Command object descriptor. More... | |
| struct | tivx_obj_desc_queue_blocked_nodes_t |
| Data structure to get information about node blocked on this object descriptor to be ready. More... | |
| struct | tivx_obj_desc_queue_t |
| Object descriptor queue. More... | |
| struct | tivx_obj_desc_data_ref_q_t |
| Data reference queue. More... | |
| struct | tivx_obj_desc_graph_t |
| Graph object descriptor as placed in shared memory. More... | |
| struct | tivx_obj_desc_super_node_edge_t |
| Super Node edge object descriptor. More... | |
| struct | tivx_obj_desc_super_node_t |
| Super Node object descriptor. More... | |
| union | tivx_obj_desc_shm_entry_t |
| Object Descriptor Shared memory entry which can hold any of the supported object descriptor types. More... | |
| struct | tivx_obj_desc_table_info_t |
| Data structure to hold info about object descriptor table. More... | |
Defines | |
| #define | TIVX_CMD_FLAG_SEND_ACK (0x00000001u) |
| Flag to indicate if command receiver needs to ACK this command. | |
| #define | TIVX_CMD_FLAG_IS_ACK (0x00000002u) |
| Flag to indicate if this is a command or ACK for a command. | |
| #define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_ENABLE_REF_CONSUMED_EVENT (0x00000001u) |
| Data Ref Q flag to determine if ref consumed event should be sent. | |
| #define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_REF_ACQUIRED (0x00000002u) |
| Data Ref Q flag to determine if ref is acquired for this data ref q. | |
| #define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_IN_DELAY (0x00000004u) |
| Data Ref Q flag to determine if this obj desc is part of some delay. | |
| #define | TIVX_OBJ_DESC_DATA_REF_Q_FLAG_DELAY_SLOT_AUTO_AGE (0x00000008u) |
| Data Ref Q flag to determine if delay slot to which this obj desc belongs should be auto aged. More... | |
| #define | TIVX_OBJ_DESC_ID_SHIFT (12u) |
| Shift for storing Object Descriptor id in 32bit variable. | |
| #define | TIVX_OBJ_DESC_ID_MASK (0x0000FFFFu) |
| Mask for storing Object Descriptor id in 32bit variable. | |
Functions | |
| tivx_obj_desc_t * | tivxObjDescAlloc (vx_enum type, vx_reference ref) |
| Allocate a Object descriptor. More... | |
| vx_status | tivxObjDescFree (tivx_obj_desc_t **obj_desc) |
| Free a previously allocated object descriptor. More... | |
| vx_status | tivxObjDescSend (uint32_t dst_target_id, uint16_t obj_desc_id) |
| Sends a object descriptor to specified target. More... | |
| tivx_obj_desc_t * | tivxObjDescGet (uint16_t obj_desc_id) |
| Get obj descriptor corresponding to the object descriptor ID. More... | |
| vx_bool | tivxObjDescIsValidType (const tivx_obj_desc_t *obj_desc, tivx_obj_desc_type_e type) |
| Checks if object desc pointer is valid and it is of required type. | |
| void | tivxObjDescInit (void) |
| Init object descriptor module. | |
| uint16_t | tivxReferenceGetObjDescId (vx_reference ref) |
| Function to get the descriptor object from the given reference. | |
| #define TIVX_OBJ_DESC_DATA_REF_Q_FLAG_DELAY_SLOT_AUTO_AGE (0x00000008u) |
Data Ref Q flag to determine if delay slot to which this obj desc belongs should be auto aged.
Valid only when TIVX_OBJ_DESC_DATA_REF_Q_FLAG_IS_IN_DELAY is set
Definition at line 129 of file tivx_obj_desc_priv.h.
| tivx_obj_desc_t* tivxObjDescAlloc | ( | vx_enum | type, |
| vx_reference | ref | ||
| ) |
Allocate a Object descriptor.
| type | [in] Type of object descriptor to allocate, see tivx_obj_desc_type_e |
| ref | [in] vx_reference that is associated with this object descriptor. If not applicable set to NULL |
| vx_status tivxObjDescFree | ( | tivx_obj_desc_t ** | obj_desc | ) |
Free a previously allocated object descriptor.
| [in] | obj_desc | Object descriptor to free |
| vx_status tivxObjDescSend | ( | uint32_t | dst_target_id, |
| uint16_t | obj_desc_id | ||
| ) |
Sends a object descriptor to specified target.
The API does not wait for ACK. ACK handling if any is done by user The API may result in a IPC is target is on another CPU Source target ID is not required since ACK is not handled by this API
| [in] | dst_target_id | Destination target ID |
| [in] | obj_desc_id | Object descriptor ID |
| tivx_obj_desc_t* tivxObjDescGet | ( | uint16_t | obj_desc_id | ) |
Get obj descriptor corresponding to the object descriptor ID.
If obj_desc_id is invalid or out of bounds NULL is returned.
| [in] | obj_desc_id | Object descriptor ID |