![]() |
TIOVX User Guide
|
Object Descriptor static configuration values.
Defines | |
#define | TIVX_OBJ_DESC_QUEUE_MAX_BLOCKED_NODES (8u) |
Max nodes that can be blocked on object descriptor queue not empty. | |
#define | TIVX_OBJ_DESC_QUEUE_MAX_DEPTH (32u) |
Max elements in a object descriptor queue. | |
#define | TIVX_CMD_MAX_OBJ_DESCS (16u) |
Max object descriptors than be parameters in a command object. | |
#define | TIVX_KERNEL_MAX_PARAMS (64u) |
Max parameters in a kernel. | |
#define | TIVX_NODE_MAX_OUT_NODES (8u) |
Max nodes taking output form a given node. | |
#define | TIVX_NODE_MAX_IN_NODES (8u) |
Max nodes feeding input to a given node. | |
#define | TIVX_PYRAMID_MAX_LEVEL_OBJECTS (32u) |
Maximum number of objects supported in pyramid. | |
#define | TIVX_OBJECT_ARRAY_MAX_ITEMS (32u) |
Maximum number of objects supported in object array. | |
#define | TIVX_GRAPH_MAX_NODES (32u) |
Max possible nodes in graph. | |
#define | TIVX_GRAPH_MAX_SUPER_NODES (8u) |
Max possible super nodes in graph. | |
#define | TIVX_GRAPH_MAX_PIPELINE_DEPTH (16u) |
Max possible pipeline depth of a graph The max value to be set by application is (TIVX_GRAPH_MAX_PIPELINE_DEPTH-1) | |
#define | TIVX_NODE_MAX_REPLICATE (32u) |
Max number of replicated nodes. | |
#define | TIVX_OBJ_DESC_MAX_SHM_ENTRY_SIZE (640U) |
Macro to check max shared mem entry size. | |
#define | TIVX_IMAGE_MAX_PLANES (3u) |
Max possible planes of data in an image. | |
#define | TIVX_CONTEXT_MAX_TENSOR_DIMS (4) |
Max possible dimensions of data in a tensor. | |
Functions | |
void | tivxGetObjDescList (volatile uint16_t obj_desc_id[], tivx_obj_desc_t *obj_desc[], uint32_t num_desc_id) |
Function to get the pointer to object descriptors for the given object descriptor id. More... | |
void tivxGetObjDescList | ( | volatile uint16_t | obj_desc_id[], |
tivx_obj_desc_t * | obj_desc[], | ||
uint32_t | num_desc_id | ||
) |
Function to get the pointer to object descriptors for the given object descriptor id.
[in] | obj_desc_id | list of object descriptor id |
[out] | obj_desc | object descriptor pointer |
[in] | num_desc_id | number of valid entries in obj_desc_id |