PDK API Guide for J721E
|
Defines the structures / control operations that could be used to configure / control NF M2M driver.
Typical Application for the NF M2M driver is as shown below.
Vhwa_m2mNfInit || Vhwa_m2mNfAllocSl2 || FVID2_Create || IOCTL_VHWA_M2M_NF_SET_CONFIG (sets NF configuration) || FVID2_ProcessReq || Wait for completion callback || FVID2_GetProcessedReq || FVID2_close || FVID2_deInit
Go to the source code of this file.
Data Structures | |
struct | Vhwa_M2mNfConfig |
Connfiguration parameters of NF. More... | |
struct | Vhwa_M2mNfCreatePrms |
Create Parameters for NF M2M Driver. More... | |
struct | Vhwa_M2mNfInitPrms |
Init Parameters for NF M2M Driver. More... | |
struct | Vhwa_M2mNfSl2AllocPrms |
Used for allocating SL2 memory. More... | |
struct | Vhwa_M2mNfPerf |
Structure for storing the performance numbers. More... | |
struct | Vhwa_M2mNfPsaSign |
Structure for storing PSA signatures. More... | |
Macros | |
#define | VHWA_M2M_NF_DRV_INST_ID (0U) |
#define | VHWA_M2M_NF_MAX_HANDLES (4u) |
Max Number of handles supported by NF M2M Driver. More... | |
#define | VHWA_M2M_NF_MIN_RD_BUFFER_DEPTH (6U) |
Minimum supported depth value for read buffer in VHWA memory. More... | |
#define | VHWA_M2M_NF_MIN_WR_BUFFER_DEPTH (2U) |
Minimum supported depth value for write buffer in VHWA memory. More... | |
#define | VHWA_M2M_NF_MAX_COMP (2u) |
Maximum possible NF iteration for a simgle request (Luma + Chroma) More... | |
#define | VHWA_NF_DEF_WIDTH (1920U) |
Default width - Used to initialize configuration parameters. More... | |
#define | VHWA_NF_DEF_HEIGHT (1080U) |
Default Height - Used to initialize configuration parameters. More... | |
Ioctls for the NF memory to memory driver | |
#define | IOCTL_VHWA_M2M_NF_SET_PARAMS (VHWA_IOCTL_M2M_NF_IOCTL_BASE) |
IOCTL for setting NF configuration. This IOCTL takes NF Configuration Nf_Config as input. More... | |
#define | IOCTL_VHWA_M2M_NF_SET_FILTER_COEFF (IOCTL_VHWA_M2M_NF_SET_PARAMS + 1U) |
IOCTL for setting the filter coefficients. More... | |
#define | IOCTL_VHWA_M2M_NF_GET_PERFORMANCE |
IOCTL for getting module's performance numbers for the last frame submitted. More... | |
#define | IOCTL_VHWA_M2M_NF_GET_PSA_SIGN |
IOCTL for getting LSE PSA Signature. More... | |
#define | IOCTL_VHWA_M2M_NF_REGISTER_ERR_CB |
IOCTL for enabling error events and registering callbacks for the same. This IOCTL pointer to Nf_ErrEventParams as input. More... | |
#define | IOCTL_VHWA_M2M_NF_SET_HTS_LIMIT |
IOCTL for enabling and setting HTS limiter. This is used to slowed down the HTS by introducing clock cycles between internal start signals. This IOCTL takes pointer to Vhwa_HtsLimiter as input. More... | |
#define | IOCTL_VHWA_M2M_NF_SYNC_START |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing. More... | |
Functions | |
int32_t | Vhwa_m2mNfInit (Vhwa_M2mNfInitPrms *nfInitPrms) |
Initializes NF Init Parameters. More... | |
void | Vhwa_m2mNfDeInit (void) |
DeInitializes NF Init Parameters. More... | |
int32_t | Vhwa_m2mNfAllocSl2 (const Vhwa_M2mNfSl2AllocPrms *sl2allocPrms) |
Function to allocate Sl2 memory for the output buffers. More... | |
void | Vhwa_m2mNfFreeSl2 (void) |
Function to free allocated SL2. More... | |
static void | Vhwa_m2mNfInitPrmsInit (Vhwa_M2mNfInitPrms *ldcCfg) |
This function should be used to initialize variable of type Vhwa_M2mNfInitPrms. More... | |
static void | Vhwa_M2mNfCreatePrmsInit (Vhwa_M2mNfCreatePrms *createArgs) |
This function should be used to initialize variable of type Vhwa_M2mNfCreatePrms. More... | |
static void | Vhwa_M2mNfSl2AllocPrmsInit (Vhwa_M2mNfSl2AllocPrms *sl2Prms) |
This function should be used to initialize variable of type Vhwa_M2mNfSl2AllocPrms. More... | |
static void | Vhwa_M2mNfConfigInit (Vhwa_M2mNfConfig *nfCfg) |
This function should be used to initialize variable of type Vhwa_M2mNfConfig. More... | |