validParams | Selection of structure parameters to be set, from the combination of Pmic_EsmCflag and the corresponding member value must be updated. |
esmDelay1_us | ESM delay-1 time interval in micro seconds. To get more effective results, user has to program esmDelay1 with multiples of 2048. The valid range is (0, 2048, 4096, 6144, 8192, ......., 522240). Valid only when PMIC_ESM_CFG_DELAY1_VALID bit is set |
esmDelay2_us | ESM delay-2 time interval in micro seconds. To get more effective results, user has to program esmDelay2 with multiples of 2048. The valid range is (0, 2048, 4096, 6144, 8192, ......., 522240). Valid only when PMIC_ESM_CFG_DELAY2_VALID bit is set |
esmHmax_us | ESM Maximum high-pulse time-threshold value in micro seconds. To get more effective results, user has to program esmHmax with multiples of 15. The valid range is (15, 30, 45, 60, 75 ....., 3840). Valid only when PMIC_ESM_CFG_HMAX_VALID bit is set |
esmHmin_us | ESM Minimum high-pulse time-threshold value in micro seconds. To get more effective results, user has to program esmHmin with multiples of 15. The valid range is (15, 30, 45, 60, 75 ....., 3840). Valid only when PMIC_ESM_CFG_HMIN_VALID bit is set |
esmLmax_us | ESM Maximum low-pulse time-threshold value in micro seconds. To get more effective results, user has to program esmLmax with multiples of 15. The valid range is (15, 30, 45, 60, 75 ....., 3840). Valid only when PMIC_ESM_CFG_LMAX_VALID bit is set |
esmLmin_us | ESM Minimum low-pulse time-threshold value in micro seconds. To get more effective results, user has to program esmLmin with multiples of 15. The valid range is (15, 30, 45, 60, 75 ....., 3840). Valid only when PMIC_ESM_CFG_LMIN_VALID bit is set |
esmErrCntThr | ESM Error count Threshold value. Valid only when PMIC_ESM_CFG_ERR_CNT_THR_VALID bit is set |
esmEnDrv | ESM ENABLE_DRV clear configuration. Valid values: Pmic_EsmEnDrvSel. Valid only when PMIC_ESM_CFG_EN_DRV_VALID bit is set |
esmMode | ESM mode select. Valid values: Pmic_EsmMode. Valid only when PMIC_ESM_CFG_MODE_VALID bit is set |