PDK API Guide for J721E
|
Input args for ENET_IOCTL_REGISTER_DSTMAC_RX_FLOW and ENET_IOCTL_UNREGISTER_DSTMAC_RX_FLOW commands.
Data Fields | |
uint32_t | coreKey |
uint32_t | startIdx |
uint32_t | flowIdx |
uint8_t | macAddress [ENET_MAC_ADDR_LEN] |
uint32_t Enet_MacDstFlowInfo::coreKey |
Core Key
uint32_t Enet_MacDstFlowInfo::startIdx |
Rx Flow Base or Start index
uint32_t Enet_MacDstFlowInfo::flowIdx |
Allocated flow's index (offset from startIdx)
uint8_t Enet_MacDstFlowInfo::macAddress[ENET_MAC_ADDR_LEN] |
Destination mac address associated with the flow