PDK API Guide for J721E
|
Enet UDMA TX channel parameters.
The structure is stripped down version of Udma_ChTxPrms
Data Fields | |
uint8_t | filterEinfo |
uint8_t | filterPsWords |
uint8_t | addrType |
uint8_t | chanType |
uint8_t | busPriority |
uint8_t | busQos |
uint8_t | busOrderId |
uint8_t | dmaPriority |
uint8_t | txCredit |
uint16_t | fifoDepth |
uint8_t EnetUdma_UdmaChTxPrms::filterEinfo |
[IN] Bool: When set (TRUE), filter out extended info
uint8_t EnetUdma_UdmaChTxPrms::filterPsWords |
[IN] Bool: When set (TRUE), filter out protocl specific words
uint8_t EnetUdma_UdmaChTxPrms::addrType |
[IN] Address type for this channel. Refer tisci_msg_rm_udmap_tx_ch_cfg_req::tx_atype
uint8_t EnetUdma_UdmaChTxPrms::chanType |
[IN] Channel type. Refer tisci_msg_rm_udmap_tx_ch_cfg_req::tx_chan_type
uint8_t EnetUdma_UdmaChTxPrms::busPriority |
[IN] 3-bit priority value (0=highest, 7=lowest)
uint8_t EnetUdma_UdmaChTxPrms::busQos |
[IN] 3-bit qos value (0=highest, 7=lowest)
uint8_t EnetUdma_UdmaChTxPrms::busOrderId |
[IN] 4-bit orderid value
uint8_t EnetUdma_UdmaChTxPrms::dmaPriority |
[IN] This field selects which scheduling bin the channel will be placed in for bandwidth allocation of the TX DMA units. Refer tisci_msg_rm_udmap_tx_ch_cfg_req::tx_sched_priority
uint8_t EnetUdma_UdmaChTxPrms::txCredit |
[IN] TX credit for external channels
uint16_t EnetUdma_UdmaChTxPrms::fifoDepth |
[IN] The fifo depth is used to specify how many FIFO data phases deep the TX per channel FIFO will be for the channel. While the maximum depth of the TX FIFO is set at design time, the FIFO depth can be artificially reduced in order to control the maximum latency which can be introduced due to buffering effects