PDK API Guide for J721E
|
Enet RM MAC address pool.
This structure has the pool of MAC addresses that are being managed.
Data Fields | |
uint32_t | numMacAddress |
uint8_t | macAddress [ENET_RM_NUM_MACADDR_MAX][ENET_MAC_ADDR_LEN] |
uint32_t EnetRm_MacAddressPool::numMacAddress |
Number of MAC addresses
uint8_t EnetRm_MacAddressPool::macAddress[ENET_RM_NUM_MACADDR_MAX][ENET_MAC_ADDR_LEN] |
Array of MAC addresses, not to exceed ENET_RM_NUM_MACADDR_MAX