PDK API Guide for J721E
|
VLAN entry type info.
Data Fields | |
CpswAle_VlanIdInfo | vlanIdInfo |
uint32_t | vlanMemberList |
uint32_t | unregMcastFloodMask |
uint32_t | regMcastFloodMask |
uint32_t | forceUntaggedEgressMask |
uint32_t | noLearnMask |
bool | vidIngressCheck |
bool | limitIPNxtHdr |
bool | disallowIPFrag |
CpswAle_VlanIdInfo CpswAle_VlanEntryInfo::vlanIdInfo |
VLAN id / VLAN type to be added
uint32_t CpswAle_VlanEntryInfo::vlanMemberList |
Port member mask for the VLAN entry being added
uint32_t CpswAle_VlanEntryInfo::unregMcastFloodMask |
Unregistered multicast flood mask - Mask used for multicast when the multicast address is not found
uint32_t CpswAle_VlanEntryInfo::regMcastFloodMask |
Registered multicast flood mask - Mask used for multicast when the multicast address is found
uint32_t CpswAle_VlanEntryInfo::forceUntaggedEgressMask |
Force untagged egress bit flags - Causes the packet VLAN tag to be removed on egress
uint32_t CpswAle_VlanEntryInfo::noLearnMask |
VLAN No Learn Mask - When a bit is set in this mask, a packet with an unknown source address received on the associated port will not be learned (i.e. When a VLAN packet is received and the source address is not in the table, the source address will not be added to the table)
bool CpswAle_VlanEntryInfo::vidIngressCheck |
VLAN Ingress Check - When set, if the receive port is not a member of this VLAN then the packet is dropped
bool CpswAle_VlanEntryInfo::limitIPNxtHdr |
Limit IP NXT hdr field - When set IP packets only with configured NXTHDR will be allowed
bool CpswAle_VlanEntryInfo::disallowIPFrag |
VLAN No IPv4 Fragmented frames Control - Causes IPv4 fragmented IP frames to be dropped